変調器 & 復調器
カテゴリー内の製品
関連資料

ビデオ
. 2025年03月17日
09:33Digital Factory of the Future
Application Note
.2025年03月11日
AN-1390: Manual Band Selection for PLL Lock Time Reduction
Application Note
.2025年02月03日
AN-920: Gain, LO, and Phase Compensation in a Single Sideband Transmitter Using the AD9788 TxDAC and ADL5372 Quadrature Modulator
Application Note
.2025年01月21日
AN-2547: Providing Fixed Power Gain at the Output of an IQ Modulator

ビデオ
. 2024年11月20日
Industrial Sustainability - The Time for Action is Now!
Application Note
.2024年09月04日
AN-2566:DAC サンプル・クロックとIQ 変調器のLO 生成に単一の外部周波数リファレンスを使用した高ダイナミック・レンジRF トランスミッタのシグナル・チェーン
Application Note
.2024年08月19日
AN-2537: An IQ Demodulator-Based IF-to-Baseband Receiver with IF and Baseband Variable Gain and Programmable Baseband Filtering
Application Note
.2024年07月12日
AN-1039: Correcting Imperfections in IQ Modulators to Improve RF Signal Fidelity
Application Note
.2024年06月06日
AN-2536: Wideband LO PLL Synthesizer with Simple Interface to Quadrature Demodulators
Application Note
.2024年01月11日
AN-0996: The Advantages of Using a Quadrature Digital Upconverter (QDUC) in Point-to-Point Microwave Transmit Systems
関連ツール
ADIsimPLL™
ADIsimPLL™
ADIsimPLLは、アナログ・デバイセズの新しい高性能PLL製品の迅速で信頼性の高い評価を可能にします。これは、現在利用できる最も包括的なPLLシンセサイザ設計およびシミュレーション・ツールです。実施されるシミュレーションには、PLL性能に影響を与える重要な非線形効果がすべて含まれます。ADIsimPLLは、設計プロセスから1回以上の反復作業を削除し、設計から市場投入までの時間を短縮します。
ADIsimRF
ADIsimRF
ADIsimRFは使いやすいRFシグナル・チェーン計算ツールです。最大50段までのシグナル・チェーンについて、カスケード・ゲイン、ノイズ、歪み、消費電力を計算し、プロット、エクスポートが可能です。ADIsimRFには、アナログ・デバイセズのRFおよびミックスド・シグナル部品のデバイス・モデルの広範なデータ・ベースも含まれています。