AD4858FMCZ Unboxing Video

2024-06-28

The EVAL-AD4858FMCZ is designed to demonstrate the performance of the AD4858 and provide access to many included configuration options that are accessed via an easy to use ACE plug-in graphical interface. The AD4858 is a fully buffered, 8-channel simultaneous sampling, 20-bit, 1 MSPS data acquisition system (DAS) with differential, wide common mode range inputs.

The EVAL-AD4858FMCZ on-board components include also the following:

  • The LTC6655 high precision, low drift, 4.096 V voltage reference (not used by default)
  • The LT1761, low noise, 1.8 V, 2.5 V, and 5 V low dropouts (LDOs)
  • The LT8330 low quiescent current (IQ) boost converter

This video provides details on how to get started using the EVAL-AD4858FMCZ evaluation platform hardware and software. For additional information, see the AD4858 data sheet and user guide, which should be consulted in conjunction with this video when using the EVAL-AD4858FMCZ.

AD4858FMCZ Unboxing Video

2024-06-28

The EVAL-AD4858FMCZ is designed to demonstrate the performance of the AD4858 and provide access to many included configuration options that are accessed via an easy to use ACE plug-in graphical interface. The AD4858 is a fully buffered, 8-channel simultaneous sampling, 20-bit, 1 MSPS data acquisition system (DAS) with differential, wide common mode range inputs.

The EVAL-AD4858FMCZ on-board components include also the following:

  • The LTC6655 high precision, low drift, 4.096 V voltage reference (not used by default)
  • The LT1761, low noise, 1.8 V, 2.5 V, and 5 V low dropouts (LDOs)
  • The LT8330 low quiescent current (IQ) boost converter

This video provides details on how to get started using the EVAL-AD4858FMCZ evaluation platform hardware and software. For additional information, see the AD4858 data sheet and user guide, which should be consulted in conjunction with this video when using the EVAL-AD4858FMCZ.