ADGM1144: 0 Hz/DC to 18 GHz, SP4T, MEMS Switch with the ADP7142 Linear Regulator
2023年07月13日
Pair the ADGM1144 Wideband MEMS Switch with the ADP7142 a CMOS, low dropout (LDO) linear regulator that operates from 2.7 V to 40 V and provides up to 200 mA of output current.
ADGM1144: 0 Hz/DC to 18 GHz, SP4T, MEMS Switch with the ADP7142 Linear Regulator
2023年07月13日
Pair the ADGM1144 Wideband MEMS Switch with the ADP7142 a CMOS, low dropout (LDO) linear regulator that operates from 2.7 V to 40 V and provides up to 200 mA of output current.
製品カテゴリ