Using Linear Regulators as a Filter

May 1 2024

Figure 1

   

Abstract

Different circuits can be used to filter a supply voltage. This article explains the main differences between using an LC filter and a linear regulator for filtering.

Introduction

Linear regulators convert a higher voltage into a lower voltage. This generated voltage is precisely regulated to an adjustable value. In this way, supply voltages for a wide variety of applications can simply be generated. However, due to their relatively low efficiency, linear regulators have been replaced with switch-mode power supplies (SMPS) in many applications. Figure 1 shows a simple linear regulator circuit for voltage conversion.

Figure

Figure 1. A simple linear regulator to convert a higher voltage to a lower voltage.

In recent years, linear regulators have found new main applications, particularly in supply line filtering. Figure 2 shows a passive filter option utilizing an LC filter, which consists of a capacitor and a coil. This type of filter is preferred due to its low direct current (DC) losses, primarily attributed to the series resistance (DCR) of the coil L. Figure 2 shows such an LC filter.

Figure

Figure 2. A filter circuit with an LC filter to reduce the voltage ripple of an SMPS.

The effectiveness of this filter depends on its transfer function, characterized by the double pole position in the Bode plot. The gain decreases at 40 dB per decade from the corner frequency, determined by the values of L and C. This filter acts as a low-pass filter, allowing DC voltages to pass through while attenuating higher frequency interference, such as voltage ripple on the supply line.

Unlike active circuitry, this filter does not require active components but relies on a coil and a capacitor. Depending on the necessary current rating and inductance of the coil, it can be quite costly.

Figure 3 shows a linear regulator used as a filter to minimize the voltage ripple of an SMPS. The effectiveness of this filter depends on the power supply rejection ratio (PSRR), which is typically represented in a graph against frequency. A good PSRR value for a linear regulator is up to 80 dB attenuation at typical switching regulator frequencies of 1 MHz.

replaceHere"

Figure. 3. A linear regulator for filtering.

The LT3042 shown is a linear regulator, which is particularly suitable as a filter stage, as it offers a high PSRR even at high frequencies and causes only very little interference of its own. This is especially important in applications where a filter is required to clean a supply voltage.

There are different ways to implement a filter, and one significant advantage of using a linear regulator for filtering is its precise regulation of the output voltage. An LC filter lacks its own voltage regulation loop, causing the generated voltage to be influenced by the behavior of the original voltage source, such as an SMPS. Depending on the DC current flow through the LC filter (shown in Figure 2), the coil’s DCR can impact the output voltage to varying degrees. While this behavior may be acceptable for applications with constant load current, it can pose challenges in applications with varying load currents.

Conclusion

To evaluate the advantages and disadvantages of different filter implementations for specific applications, simulation tools may be highly beneficial. LTspice® is a free and effective simulation tool that can assist in this process.

About the Authors

Frederik Dostal
Frederik Dostal is a power management expert with more than 20 years of experience in this industry. After his studies of microelectronics at the University of Erlangen, Germany, he joined National Semiconductor in 2001, w...

Related to this Article

Product Categories

Latest Media 21

Subtitle
Learn More
3