How to Select Supply Topology for Processors, Microcontrollers, and High Power Devices

Figure 1

   

Abstract

This article provides a comprehensive guide on how to select the right power supply topology for processors, microcontrollers, and high power signal chains. It highlights the critical role of efficient and reliable power conversion in the signal chain and emphasizes the significance of these compact yet powerful devices across diverse electronic applications. Whether in consumer or industrial automation settings, these devices act as primary processing units, necessitating a stable and precisely regulated power supply for optimal performance. The guide underscores the importance of choosing a suitable power supply architecture to ensure seamless and optimal operation.

Introduction

This article will delve into the practical considerations of power supply topologies (low dropout (LDO) regulator, buck, boost, buck-boost, and single input multiple output (SIMO)). It will assess their applications, significance, benefits, and drawbacks. By providing practical insights, this evaluation aims to assist in making informed decisions during the design process.

The Importance of Core Voltage Stability

Before delving into the details of power supply topologies, it is crucial to understand the significance of maintaining core voltage stability for processors and microcontrollers.

  • Performance: A stable core voltage ensures consistent and reliable performance of the device, preventing unexpected crashes, glitches, or erratic behavior.

  • Power efficiency: Well-regulated core voltage minimizes power wastage, enhancing the overall energy efficiency of the system.

  • Longevity: Voltage fluctuations can lead to premature wear and tear on the device, reducing its lifespan.

  • Electromagnetic compatibility (EMC): Stable core voltage helps meet EMC standards by reducing electromagnetic interference (EMI), which is essential in sensitive applications like medical devices and aerospace systems.

  • Noise immunity: Proper voltage regulation protects the device from external electrical noise, enhancing its reliability in noisy environments.

Common Power Supply Topologies

Commonly used power supply topologies for microprocessors and microcontrollers include linear regulators and switched-mode power supplies (SMPS) like buck, boost, buck-boost converters, and SIMO converters. Each topology has its own advantages and disadvantages. Let’s delve into these topologies to gain a thorough understanding.

Linear Regulator

Linear regulators are simple and cost-effective solutions for low power applications. They work by dissipating excess voltage as heat, providing a constant output voltage regardless of input variations. However, they are inefficient for high current applications because of the power dissipation. Figure 1 shows a linear regulator.

Figure 1. The ADP7142, a linear regulator for a 1.8 V output rail.

There are many things to consider when designing with LDO regulators. Table 1 outlines the advantages and disadvantages.

Table 1. LDO Advantages and Disadvantages
Advantages Disadvantages
LDO regulators maintain stable output
voltage even with input voltages close
to the desired level, ensuring reliable
performance with low input power.
LDO regulators lose efficiency when
the input and output voltages differ
significantly, resulting in excess power
being converted into heat. In such cases,
switching regulators may be a more
energy-efficient choice.
With minimal output noise, LDO regulators
excel in applications demanding a clean
and stable voltage supply, such as
precision analog circuits and sensitive
microcontrollers.
LDO regulators have lower currenthandling capabilities compared to
switching regulators, making them
unsuitable for high power applications or
those with heavy current demands.
LDO regulators simplify designs by
requiring fewer external components
compared to alternatives like switching
regulators, resulting in a compact PCB
footprint and reduced complexity.
LDO regulators tend to generate heat
due to power dissipation, especially in
high power situations. Proper thermal
management is crucial to prevent
overheating.
Offering swift responses to load changes,
LDO regulators are ideal for applications
with dynamic conditions, such as
microcontrollers and digital processors.
LDO regulators require an input voltage
higher than the desired output, limiting
their use in battery-powered devices
where the battery voltage is close to the
desired output.
Ultralow quiescent current versions of
LDO regulators enhance efficiency for
battery-powered devices, minimizing
standby power consumption.
While LDO regulators can be cost-effective
in many scenarios, they may not be the
most budget-friendly choice for high
current or high efficiency applications
compared to switching regulators.
LDO regulators have excellent output
voltage accuracy, making them wellsuited for applications requiring precise
voltage regulation.
If the input voltage is significantly higher
than the desired output, LDO regulators
may require additional components such
as heat sinks or complex protection
circuits to function effectively.

Switched-Mode Power Supply (SMPS)

SMPS is the most commonly used topology for microprocessors and microcontrollers due to their high efficiency. An SMPS converts the input voltage to the desired output by rapidly switching the power devices (usually transistors) on and off. This allows for precise voltage regulation and minimizes power dissipation. Buck, boost, and buck-boost topologies are demonstrated in Figure 2.

Figure 2. Buck, boost, and buck-boost compose the fundamental SMPS topologies.1

When utilizing an SMPS, various factors should be considered, including both advantages and disadvantages. Table 2 outlines these important aspects.

Table 2. SMPS Advantages and Disadvantages
Advantages Disadvantages
SMPS excels in efficiency, wasting
less power as heat compared to linear
regulators, making it an ideal solution
for energy-efficient devices and those
powered by batteries.
Designing and implementing SMPS is
more intricate than linear regulators,
demanding extra components and
advanced control circuitry. This
complexity can raise development costs
and pose reliability challenges.
With the ability to handle a broad input
voltage range, SMPS is well-suited for
applications dealing with fluctuating or
unstable power sources.
SMPS can result in EMI, impacting nearby
components. As such, additional filtering
and shielding measures are needed to
mitigate potential issues.
Compact and lightweight, SMPS outshines
linear power supplies in size and weight,
making it a top choice for applications
with critical constraints.
Certain SMPS designs may exhibit
higher output voltage ripple than linear
regulators, posing a challenge for
applications demanding ultralow noise
levels.
Offering stable output voltage even with
varying or inconsistent input, SMPS plays
a vital role in powering electronic devices
reliably.
Despite its efficiency, SMPS can be pricier
to manufacture and design due to the
need for additional components and
control circuitry.
SMPS boasts a quick transient response,
making them the go-to for applications
requiring swift adjustments to load
changes.
SMPS may not be a one-size-fits-all
solution, particularly in scenarios where
electrical noise or interference is a
concern, or when a pristine DC output is
essential.
Versatility is a key strength of SMPS, as it
can be tailored to meet a wide range of
output voltage and current requirements,
catering to diverse applications.
Some SMPS designs have limitations on
the maximum current they can handle. For
high power applications, larger and more
complex SMPS systems may be necessary.
Generating minimal heat, SMPS is
advantageous in applications where
effective thermal management is a
priority.
 

Types of SMPS

Buck Converter

A buck converter is a specific type of SMPS that steps down the input voltage to a lower output voltage. It is widely used for powering microcontrollers and low power microprocessors. The buck converter operates by turning the switch (usually a transistor) on and off, storing energy in an inductor and capacitor, and then delivering it to the output in a regulated manner. Figure 3 depicts a buck converter utilized in a system-level solution to convert a high voltage rail to 3.3 V efficiently.

Figure 3. The LT8631 micropower buck converter solution.

When opting for a buck converter as the power supply topology, it’s essential to weigh its advantages and disadvantages. Table 3 provides a summary overview of these key considerations.

Table 3. Buck Converter Advantages and Disadvantages
Advantages Disadvantages
Buck converters are known for their high 
efficiency when converting higher input 
voltages to lower output voltages. They 
waste less energy as heat compared to 
linear regulators.
Buck converters require complex control 
circuitry for proper operation, which can 
increase design complexity and the risk of 
potential reliability issues.
Thanks to their high efficiency, buck 
converters generate less heat, which is 
crucial for applications where thermal 
management is a concern.
Buck converters can generate EMI due 
to the switching action, which may 
require additional filtering and shielding 
measures.
Buck converters are typically smaller and 
lighter than linear regulators, making 
them suitable for applications with size 
and weight constraints.
Some buck converter designs may have a 
higher output voltage ripple compared to 
linear regulators. This can be a concern 
for applications that require very low 
noise levels.
Buck converters can handle a broad input 
voltage range, allowing them to work well 
with variable or unstable power sources.
Buck converters can only step down the 
input voltage, and they are not suitable for 
applications that require a higher output 
voltage than the input voltage.
Buck converters have a fast transient 
response, making them suitable 
for applications that require rapid 
adjustments to changes in load 
conditions.
Some buck converter designs have 
limitations in terms of the maximum 
current they can handle. High power 
applications may require more complex 
buck converter configurations.
Buck converters provide a stable and well regulated output voltage, even when the 
input voltage fluctuates.
The design and selection of components 
for a buck converter can be challenging 
and may require careful consideration 
of factors such as inductor selection, 
switching frequency, and control loop 
design.
Buck converters are commonly used in 
battery-powered devices where energy 
efficiency is critical. They help extend 
battery life by minimizing power losses.

SIMO Converter

SIMO is an innovative power management technique that provides multiple regulated voltage outputs from a single inductor.2 Traditional power management circuits typically require a separate inductor for each output, leading to increased component count, board space, and energy losses. SIMO simplifies this by using a single inductor shared between multiple output channels, improving efficiency, and reducing the overall footprint. A SIMO design used to power up multiple output rails is illustrated in Figure 4.

Figure 4. The MAX17270 SIMO converter configured to have three output rails.

When employing the SIMO converter as a power supply topology, it’s important to consider various factors. Table 4 concisely outlines the advantages and disadvantages of this choice.

Table 4. SIMO Converter Advantages and Disadvantages
Advantages Disadvantages
SIMO technology boosts power efficiency 
by sharing a single inductor among 
multiple outputs, cutting energy losses—a 
win for battery-powered devices.
Implementing SIMO brings complexity 
in control and regulation compared to 
traditional power solutions. Achieving 
stability and reliability for multiple outputs 
demands meticulous design and control 
circuitry.
Using just one inductor for multiple 
outputs, SIMO trims down the PCB 
footprint, a major plus for compact and 
space-limited applications.
SIMO usually supports a limited number 
of output channels due to sharing a 
single inductor, making it less suitable for 
applications needing numerous voltage 
levels.
With fewer components and simpler 
circuitry, SIMO brings cost savings in 
manufacturing, reducing the risk of faults 
and enhancing device reliability.
SIMO designs may struggle to swiftly 
respond to rapid load changes, as the 
shared inductor adjusts to diverse output 
voltage requirements.
Thanks to improved efficiency, SIMO 
designs generate less heat, keeping 
operating temperatures cooler and 
potentially extending device lifespan, 
without the need for complex thermal 
management.
Engineers face a delicate balance in SIMO 
designs, weighing the number of output 
channels, efficiency, and component 
count. Navigating this trade-off for a 
specific application can be a challenge.
SIMO technology crafts compact and 
energy-efficient power solutions, making 
it perfect for wearables, IoT devices, and 
smartphones.
Adapting existing devices to SIMO 
technology may require substantial 
redesign and redevelopment, posing 
potential hurdles for seamless integration.

Boost Converter

A boost converter is a power supply topology that steps up the input voltage to a higher output voltage. While less common for microcontrollers and microprocessors, boost converters find use in applications where a higher core voltage is needed. In Figure 5, a boost converter is used to provide a 24 V output rail of a high voltage precision amplifier.

Figure 5. The LT8336, boost converter with an output voltage of 24 V.

When opting for a boost converter as your power supply topology, it’s crucial to consider several factors. Table 5 provides a clear overview of the advantages and disadvantages associated with this choice.

Table 5. Boost Converter Advantages and 
Disadvantages
Advantages Disadvantages
Ideal for high voltage applications: 
Boost converters are well-suited for 
applications that require a higher 
output voltage than the input voltage.
Less efficient than buck converters: Boost 
converters typically have lower efficiency 
compared to buck converters, as they need to 
step up the voltage.
Efficiently boosts input voltage: Boost 
converters can efficiently increase 
the input voltage to the desired 
output voltage level.
Not recommended for battery-powered 
devices that prioritize energy efficiency: Boost 
converters may not be the best choice for 
battery-powered devices that prioritize energy 
efficiency, as they consume more power and 
may drain the battery faster.

Buck-Boost Converter

The buck-boost converter combines the capabilities of both buck and boost converters, allowing it to step down or step up the input voltage to provide a regulated output voltage. This flexibility makes it a versatile choice for applications with varying voltage requirements. For example, in Figure 6, a buck-boost converter is used to regulate the output voltage from a battery cell stack that can have varying input voltages. Once the battery stack is in charge operation (the input voltage is roughly around 4.5 V to 5 V while in discharge operation) the battery cell voltage may drop to 1.5 V to 2.7 V, therefore a buck-boost converter is required for this type of application.

Figure 6. The LTC3114-1, buck-boost converter configured to have an output voltage of 3.3 V.
Figure 7. The LT8631 buck converter performance generated by the LTpowerCAD® program.

When using a buck-boost converter as your power supply architecture, you must consider several factors. Table 6 briefly summarizes the benefits and drawbacks of this option.

Table 6. Buck-Boost Converter Advantages and 
Disadvantages
Advantages Disadvantage
Versatile for various input and output 
voltages: The buck-boost converter 
can handle a wide range of input and 
output voltages, making it suitable 
for applications with different power 
requirements.
Moderately complex compared to simpler 
converters: The buck-boost converter 
is more complex than simpler converter 
topologies like the buck or boost 
converter. This complexity may require 
additional design considerations and 
careful component selection. 
Ideal for battery-powered devices, 
working from a single power source: Since 
the input voltage can vary significantly in 
battery-powered devices, the buck-boost 
converter can efficiently regulate the 
output voltage regardless of the battery’s 
charge level.
 
Works from a single power source: The 
buck-boost converter can operate from a 
single power source, making it suitable for 
applications where only one power supply 
is available.
 

Factors to Consider When Choosing a Topology

Selecting the right power supply topology for your microprocessor or microcontroller depends on various factors. Here are some key considerations:

  • Power efficiency: Determine the power requirements of the device and choose a topology that offers high efficiency to minimize energy consumption and heat generation.

  • Input voltage range: Consider the range of input voltages the device may encounter in its operating environment. Ensure that the chosen topology can accommodate these variations.

  • Output voltage: Determine the required core voltage for the microprocessor or microcontroller. Some topologies, like buck-boost converters, are more flexible in this regard.

  • Size and weight constraints: If the application has space or weight limitations, choose a topology that offers a compact and lightweight solution.

  • Cost: Evaluate the cost constraints of the project. While linear regulators may be cost-effective for low power applications, SMPS solutions might be more cost-efficient for higher power requirements.

  • EMC considerations: If the application requires compliance with EMC standards, ensure that the chosen topology can meet these requirements through proper layout and filtering.

  • Transient response: Consider the transient response of the power supply. Microprocessors and microcontrollers often experience sudden changes in load, and topology with a fast and stable response is essential to prevent voltage droop or overshoot.

  • Reliability: Assess the reliability requirements of the application. Some topologies, like linear regulators, have fewer components and may be more reliable in certain scenarios.

  • Environmental conditions: Take into account the operating environment of the device. For battery-powered applications, energy efficiency is crucial, while for industrial applications, robustness, and noise immunity may be more critical.

Practical Tips for Implementation

Once you have selected the appropriate power supply topology, here are some practical tips for successful implementation:

  • Component selection: Choose high quality components, including inductors, capacitors, and transistors, to ensure stable and reliable operation.

  • Layout and routing: Pay careful attention to the layout and routing of the power supply circuitry on your PCB. Minimize loop areas and use proper grounding techniques to reduce noise and improve EMC performance.

  • Filtering: Incorporate input and output filters as needed to suppress EMI and ensure a clean and stable output voltage.

  • Protection: Implement overvoltage, undervoltage, and overcurrent protection mechanisms to safeguard the microprocessor or microcontroller from potential damage.

  • Testing and characterization: Thoroughly test and characterize your power supply circuit under various operating conditions to ensure it meets the desired performance specifications.

  • Heat management: If the design involves power dissipation, consider adding heat sinks or thermal management solutions to prevent overheating.

Conclusion

Choosing the right power supply topology for a microprocessor or microcontroller is a crucial step in the design process. Each topology offers a unique set of advantages and disadvantages, and the decision should be based on the specific requirements of your application. Factors such as power efficiency, input voltage range, and output voltage stability should be considered to make an informed choice that ensures the reliable and efficient operation of the device.

However, it’s important to note that the implementation phase is equally important. Proper component selection, careful layout and routing, and thorough testing are essential to realizing the full potential of a chosen power supply topology. By paying attention to these details, microprocessors and microcontrollers can be powered effectively, enabling them to perform at their best in a wide range of applications.

References

An Introduction to Switch-Mode Power Supplies.” Maxim’s Engineering Journal, Vol. 61, September 2007.

Cary Delano and Gaurav Mital. “SIMO Switching Regulators: Extending Battery Life for Hearables and Wearables.” Maxim Integrated (Now Analog Devices, Inc.), November 2017.

About the Authors

Jan Michael Gonzales
Jan Michael Gonzales is a product applications engineer for power systems at Analog Devices Philippines. He joined ADI in 2020 and is primarily working on powering precision signal chains. He received a bachelor’s degree i...
Ralph Clarenz Matociños
Ralph Clarenz Matociños graduated with a bachelor’s degree in electronics engineering from Pamantasan ng Lungsod ng Maynila (PLM) in Manila, Philippines. He has over one year of engineering experience in power electronics,...
Christian Cruz
Christian Cruz is a staff applications development engineer at Analog Devices, Inc., Philippines. He holds a bachelor’s degree in electronics engineering from the University of the East in Manila, Philippines. He has more ...

Latest Media 21

Subtitle
Learn More
Add to myAnalog

Add article to the Resources section of myAnalog, to an existing project or to a new project.

Create New Project