LTspice: Using an Intrinsic Symbol for a Third-Party Model

2014-09-09

LTspice IV can automatically create a symbol for a third-party model, or you can associate a third-party subcircuit with an LTspice intrinsic symbol, as long as the third-party .SUBCKT model and the intrinsic symbol share an identical pin/port netlist order. For example, to add an N-channel MOSFET transistor symbol to a schematic and define it with an IRF_7401 .SUBCKT statement:

  1. Add an instance of the N-channel MOSFET transistor symbol to your schematic.
  2. Move the cursor over the body of the MOSFET symbol and Ctrl + Right-Click. A dialog box appears.
  3. Change Prefix: “MN” to “X”. The symbol now netlists as a subcircuit instead of an intrinsic NMOS transistor.
  4. Change “NMOS” to be “IRF_7401”, corresponding to the name on the .SUBCKT line.
  5. Click OK.
  6. Either add the .SUBCKT IRF_7401 lines to your schematic or reference the library containing it (.INCLUDE third_party.lib) as a SPICE directive.

Again, this assumes the third-party model you’re adding follows popular pin order conventions. When in doubt, use the automatic symbol generation feature because it takes care of any discrepancies with regard to pin and port netlist order. For more about automatic symbol generation, see Help > Schematic Capture > Creating New Symbols > Automatic Symbol Generation.

关于作者

Gabino Alonso
Gabino Alonso目前是Power by Linear™部门的战略营销总监。加入ADI公司之前,Gabino在凌力尔特、德州仪器、加州理工州立大学担任过市场营销、工程、运营和讲师等多个职位。他拥有加州大学圣巴巴拉分校电子和计算机工程硕士学位。
添加至 myAnalog

作者联系方式

Gabino Alonso

电源战略营销总监

关联至此文章

资源

最新视频 20

Subtitle
了解更多
添加至 myAnalog