MAX6951/MAX6950 LED显示驱动器与MAXQ2000微控制器的通信
Abstract
本应用笔记说明MAX6951/MAX6950 LED驱动器和MAXQ2000的SPI外设通信的汇编程序设计。
引言
MAX6950和MAX6951分别为5位和8位共阴极LED显示驱动器,通过高速SPI 接口控制。这两款器件采用独特的复用结构,大大减少了LED驱动器与LED面板的连线。MAXQ2000是一款高性能、16位RISC微控制器,集成了SPI模块,简化了LED驱动器与微控制器的连接。本应用笔记提供了MAXQ®汇编程序范例,说明MAXQ2000 SPI模块与MAX6951/MAX6950的配合使用。
硬件和软件需求
为了实现本应用笔记的接口试验,需要MAX6951评估板(EV kit)、MAXQ2000评估板(包括MAX-IDE软件)、科提供最小200mA电流的+5V电源和具备一个可用串口的PC机。
硬件设置
- MAX6951评估板跳线设置
去掉JU2、JU3和JU4引脚1与引脚2之间的跳线,断开/CS\、DIN和SCLK信号与评估板上电平转换器的连接。 - MAXQ2000评估板跳线和DIP开关设置
开关SW3的1-8引脚置于off位置
JU1:连接引脚1和引脚2
JU2:连接引脚1和引脚2
JU3:连接引脚1和引脚2
JU4:开路
JU10:开路
JU11:接通(MAXQ2000评估板由一块JTAG接口板供电,电源为+5V。) - 按图1所示连接两块评估板。

图1. MAX6951评估板与MAXQ2000评估板的连接图
固件说明
可从Maxim网站下载本项目的完整固件文件,通过Maxim提供的集成开发环境和调试环境,用于MAXQ系列微控制器的MAX-IDE,进行编译。
下载:完整的固件(ZIP, 18.8k)
main.asm文件
该文件为本项目的主循环程序,它通过调用不同的子程序演示正确写入MAX6951寄存器的数据。固件演示MAX6951的以下功能:
- MAX6951 SPI接口初始化。
- 在16进制译码方式下,对MAX6951所有数字的P0和P1级写入并显示0、1、2、...、A、B、C、D、E、F和8个小数位(如,点亮所有LED字段)。
- 在非译码方式下,写入并显示上述字母和其它用户内建字符,如H、L、P、Q、Y等。
- LED亮度调节,该程序说明如何设置MAX6951亮度寄存器,测试数字亮度控制功能。
- 扫描限制循环程序。该程序用相同亮度循环显示第1位到第8位数字。
注:监控进程,以确认扫描限制提高时,降低亮度。 - 闪烁控制,该程序将不同数值写入每位数据的P0级和P1级。还可采用快速闪烁方式来演示段闪烁控制功能,可同步多个LED驱动器。
- 滚动循环,该程序从左到右、从右到左滚动显示文本信息:HELLO。
- 跳动循环,该程序在LED两个边沿之间跳动显示文本信息:HELLO。
- 计时循环,这个程序说明在16进制译码方式和非译码方式下,如何设计显示毫秒级计时。
max2000ev_6951.asm文件
该文件包含所有用于MAX6951评估板与MAXQ2000微控制器之间通信的功能函数。其主要函数有:
- max6951_init:该函数正确地设置MAXQ2000的SPI模式,实现与MAX6951的连接。使能SPI,并初始化MAX6951,在显示板上显示八个0。列表1为该函数的详细代码。
列表1. MAX6951初始化例程
;******************************************************************************* ;* Function: max6951_init ;* ;* Sets the correct SPI modes for talking to the MAX6951, enables SPI, and ;* ;* initializes the MAX6951 to display 8 0s. ;* ;* Input: None. ;* ;* Output: None. ;* ;* Destroys: ACC, A[0] -- A[10], PSF ;* ;******************************************************************************* MAX6951_INIT: ; SET SPI BAUD RATE MOVE A[0], #2400H ; SYSTEM CLOCK IS 16,000,000 HZ MOVE A[1], #00F4H MOVE A[2], #4240H ; DESIRED BAUD RATE IS 1,000,000 HZ MOVE A[3], #000FH CALL SPI_SETBAUDRATE ; SET THE APPROPRIATE MODES FOR THE 6951 MOVE C, #SPI_IDLE_LOW ; IDLE = LOW CALL SPI_SETCLOCKPOLARITY MOVE C, #SPI_ACTIVE_EDGE ; ACTIVE = RISING EDGE CALL SPI_SETCLOCKPHASE MOVE C, #SPI_LENGTH_16 ; ALWAYS TRANSFER 16 BITS CALL SPI_SETCHARACTERLENGTH MOVE C, #SPI_MASTER_MODE ; MAXQ2000 IS THE MASTER, MAX6951 IS THE SLAVE CALL SPI_SETMODE ; ENABLE SPI MOVE C, #1 CALL SPI_ENABLE ; SHUTDOWN MAX6951 DISPLAY FIRST CALL MAX6951_SHUTDOWN ; SET MAX6951 IN HEXADECIMAL DECODE MODE MOVE ACC, #MAX6951REG_DECODE SLA4 SLA4 OR #0FFH ; HEXADECIMAL DECODE CALL MAX6951_TRANSMIT ; SET DISPLAY INTENSITY = 16/16 MOVE ACC, #MAX6951REG_INTENSITY SLA4 SLA4 OR #0FH ; INTENSITY = 16/16 CALL MAX6951_TRANSMIT ; SCAN LIMIT = 7 MOVE ACC, #MAX6951REG_SCANLIMIT SLA4 SLA4 OR #07H ; SCAN LIMIT = 7 CALL MAX6951_TRANSMIT RET
- max6951_transmit:该函数向Max6951发送一个寄存器地址和数据字节(16位)。
- max6951_set_all_n:这些函数将一位数字寄存器的P0级和P1级设置为数字“n”。所有函数具备16进制译码和非译码模式。
- max6951_e_d_s_d:该函数先使能MAX6951显示,然后延迟半秒,关断显示,再延迟100ms。
- max6951_screenshot:这些函数在8位数字LED面板的八个不同位置处显示HELLO。
- max6951_scroll_R_to_L:以不同顺序显示,该函数以非译码方式从右至左滚动显示HELLO。
- max6951_scroll_L_to_R:以不同顺序显示,该函数以非译码方式从左至右滚动显示HELLO。
- max6951_bouncing:该函数在LED的两个边沿之间跳动显示HELLO。
- font_lookup:给定一个16进制数,该函数查询在标准7段LED上以非译码方式显示的相同字符。
- max6951_counting:该函数用于显示毫秒计时,精确度为10毫秒。 列表2为详细代码。
列表2. MAX6951计时例程
;******************************************************************************* ;* Function: max6951_counting ;* ;* This routine counts how many 10-milliseconds have elapsed and displays ;* ;* the value from 0000 to 9999 on LED digits 3-0(no way to blank leading digits). ;* ; The routine displays the same value on LED digits 7-4(by using no decode ;* ;* mode, individual leading digits can be blanked). ;* ;* Input: None ;* ;* Output: None ;* ;* Destroys: ACC, A[1] - A[4], A[9] ;* ;******************************************************************************* MAX6951_COUNTING: CALL MAX6951_SHUTDOWN CALL MAX6951_SET_ALL_0 ; SET ALL BITS OF DATA REGISTERS TO 0 MOVE ACC, #010FH ; HEXDECIMAL DECODE DIGITS 3-0, NO DEOCDE DIGITS 7-4 CALL MAX6951_TRANSMIT ; INITIALIZE THE COUNT TO 0 MOVE A[1], #0 ; A[1] => DIGIT 0 MOVE A[2], #0 ; A[2] => DIGIT 1 MOVE A[3], #0 ; A[3] => DIGIT 2 MOVE A[4], #0 ; A[4] => DIGIT 3 COUNT_LOOP: INCREASE_DIGIT3: MOVE ACC, A[4] ; PROCESS DIGIT 3 SUB #9 JUMP Z, INCREASE_DIGIT2 ; DIGIT 3 = 9, THERE IS CARRY OVER MOVE ACC, A[4] ; DIGIT 3 < 9, CONTINUE ADD #1 MOVE A[4], ACC CALL FONT_LOOKUP ; LOOK UP THE VALUE FOR THIS FONT ; STORE IT IN A[9], KEEP ACC UNCHANGED OR #6300H CALL MAX6951_TRANSMIT ; NO CARRY OVER, WRITE DIGIT 3 NEW VALUE MOVE ACC, A[9] ; WRITE THE NO DECODE VALUE TO DIGIT 7 OR #6700H CALL MAX6951_TRANSMIT JUMP DISPLAY_NUMBER INCREASE_DIGIT2: OR #6300H CALL MAX6951_TRANSMIT ; WRITE 0 TO DIGIT 3 REGISTER FIRST MOVE A[4], #0 ; SET DIGIT 3 BACK TO 0 MOVE ACC, #677EH ; NO DECODE VALUE FOR FONT '0' IS "7EH" CALL MAX6951_TRANSMIT ; WRITE 7EH TO DIGIT 7 REGISTER MOVE ACC, A[3] ; PROCESS DIGIT 2 SUB #9 JUMP Z, INCREASE_DIGIT1 ; DIGIT 2 = 9, THERE IS CARRY OVER MOVE ACC, A[3] ; DIGIT 2 < 9, CONTINUE ADD #1 MOVE A[3], ACC CALL FONT_LOOKUP ; LOOK UP THE VALUE FOR THIS FONT ; STORE IT IN A[9], KEEP ACC UNCHANGED OR #6200H CALL MAX6951_TRANSMIT ; NO CARRY OVER, WRITE DIGIT 2 NEW VALUE MOVE ACC, A[9] ; WRITE THE NO DECODE VALUE TO DIGIT 6 OR #6600H CALL MAX6951_TRANSMIT JUMP DISPLAY_NUMBER INCREASE_DIGIT1: OR #6200H CALL MAX6951_TRANSMIT ; WRITE 0 TO DIGIT 2 REGISTER FIRST MOVE A[3], #0 ; SET DIGIT 2 BACK TO 0 MOVE ACC, #667EH ; NO DECODE VALUE FOR FONT '0' IS "7EH" CALL MAX6951_TRANSMIT ; WRITE 7EH TO DIGIT 6 REGISTER MOVE ACC, A[2] ; PROCESS DIGIT 1 SUB #9 JUMP Z, INCREASE_DIGIT0 ; DIGIT 1 = 9, THERE IS CARRY OVER MOVE ACC, A[2] ; DIGIT 1 < 9, CONTINUE ADD #1 MOVE A[2], ACC CALL FONT_LOOKUP ; LOOK UP THE VALUE FOR THIS FONT ; STORE IT IN A[9], KEEP ACC UNCHANGED OR #6100H CALL MAX6951_TRANSMIT ; NO CARRY OVER, WRITE DIGIT 1 NEW VALUE MOVE ACC, A[9] ; WRITE THE NO DECODE VALUE TO DIGIT 5 OR #6500H CALL MAX6951_TRANSMIT JUMP DISPLAY_NUMBER INCREASE_DIGIT0: OR #6100H CALL MAX6951_TRANSMIT ; WRITE 0 TO DIGIT 1 REGISTER FIRST MOVE A[2], #0 ; SET DIGIT 1 BACK TO 0 MOVE ACC, #657EH ; NO DECODE VALUE FOR FONT '0' IS "7EH" CALL MAX6951_TRANSMIT ; WIRTE 7EH TO DIGIT 5 REGISTER MOVE ACC, A[1] ; PROCESS DIGIT 0 SUB #9 JUMP Z, COUNT_COMPLETE ; DIGIT 0 = 9, COUNTING IS OVER MOVE ACC, A[1] ; DIGIT 0 < 9, CONTINUE ADD #1 MOVE A[1], ACC CALL FONT_LOOKUP ; LOOK UP THE VALUE FOR THIS FONT ; STORE IT IN A[9], KEEP ACC UNCHANGED OR #6000H CALL MAX6951_TRANSMIT ; NO CARRY OVER, WRITE DIGIT 0 NEW VALUE MOVE ACC, A[9] ; WRITE THE NO DECODE VALUE TO DIGIT 4 OR #6400H CALL MAX6951_TRANSMIT DISPLAY_NUMBER: ; DISPLAY DIGIT 3-0 IN HEXADECIMAL DECODE MODE ; DIEPLAY DIGIT 7-4 IN NO DECODE MODE CALL MAX6951_ENABLE CALL MAX6951_10MS_DELAY JUMP COUNT_LOOP COUNT_COMPLETE: RET
divide32.asm文件:这是MAX-IDE软件提供的32位除法程序。
maxq2000.inc、maxq2000_spi.inc和max2000ev_6951.inc文件:这些是MAXQ2000引脚定义和MAX6951寄存器定义的嵌套文件。
结论
MAX6951/MAX6950 SPI LED驱动器简单易用的共阴极显示器驱动器,通过SPI串行接口连接微控制器。MAXQ系列微控制器集成了SPI模块,可通过SPI接口与LED驱动器通信。这里介绍的例程有助于用户理解MAX6951的LED驱动功能。也可将该例程应用到类似的MAXQ2000系统开发中。