Simple Methods Reduce Input Ripple for All Charge Pumps

2003年05月13日

Figure 1

   

要約

Charge pumps are a form of DC-DC converter that rely on capacitors instead of inductors for energy storage and transfer. The absence of inductors makes them attractive in situations requiring a low-power auxiliary supply (output currents up to about 150mA). They use less circuit-board area, offer minimal component height, and are easy to use.

Charge pumps can have regulated or unregulated outputs. An unregulated charge pump either doubles or inverts the voltage that powers it and the output voltage is a function of the supply voltage. A regulated charge pump either boosts or inverts the supply voltage. Its output voltage is independent of the supply.

Techniques that reduce capacitor size and optimize output current—fast switching speed and low-on-resistance switches—also produce noise and transient ripple at the input supply pin. Noise can propagate back along the input supply pins, creating problems for crystal-controlled oscillators, VCOs, and other sensitive circuits with poor power-supply rejection. This article focuses on methods for reducing the noise.

Simplified Operation

First, consider a charge pump connected as an inverter. In the simplified version (Figure 1), operation is controlled by 2-phase clock signals with 50% duty cycles. The pump capacitor (charge-transfer component) is charged to VIN via closure of SW1A and SW1B. SW2A and SW2B are open at this time. On the next clock cycle, the closure of SW2A and SW2B connects the pump capacitor to COUT, thereby producing -VIN at the output.

Figure 1. Simplified diagram of a charge pump connected as an inverter.

Figure 1. Simplified diagram of a charge pump connected as an inverter.

Next, connect the charge pump as a doubler (Figure 2). As before, operation is controlled by 2-phase, 50%-duty-cycle clock signals. The pump capacitor is the charge transfer device and is charged up to VIN by closure of SW2A and SW2B (SW1A and SW2B are open at this time). On the next clock cycle, the closure of SW1A and SW1B produces +2VIN at the output by connecting the pump capacitor to COUT.

Figure 2. Simplified diagram of a charge pump connected as a doubler.

Figure 2. Simplified diagram of a charge pump connected as a doubler.

Input and output ripple is caused by rapid charging and discharging of the pump capacitor. An inverter circuit (Figure 3) built around the MAX665 charge pump and producing 5V across 51Ω, illustrates the input-ripple artifacts (Figure 4). (Ripple produced by the high-current, low-frequency (≤ 100kHz) MAX665 is easily measured.)

Figure 3. This charge-pump inverter circuit is used for measurements.

Figure 3. This charge-pump inverter circuit is used for measurements.

Figure 4. Input voltage and current ripple for standard inverter circuit: CIN = C<sub loading=PUMP = COUT = 100µF, RLOAD = 51ohm, VIN = +5.73V, and VOUT = -5.06V. Input current ripple (upper trace): 100mA/div. Input voltage ripple (lower trace): 200mV/div, AC coupled." class="img-responsive">

Figure 4. Input voltage and current ripple for standard inverter circuit: CIN = CPUMP = COUT = 100µF, RLOAD = 51Ω, VIN = +5.73V, and VOUT = -5.06V. Input current ripple (upper trace): 100mA/div. Input voltage ripple (lower trace): 200mV/div, AC coupled.

Ripple-reduction Methods

To reduce ripple, you must isolate ripple sources from the rest of the circuit. For best conversion efficiency in the charge pump, you should also minimize ESR and ensure that the input-, output-, and pump-capacitor values are as close as possible to those recommended in the data sheet. The following discussion covers four techniques for minimizing ripple and its effects.

  1. Reducing ESR in the input capacitor implies multiple capacitors connected in parallel: N identical capacitors in parallel reduces the input ripple by N-1. Unfortunately, that approach is not very effective in terms of cost and pc-board area.
  2. Instead, add an LC filter at the input supply pin (Figure 5). The additional filtering prevents ripple from propagating to other circuits via the input supply trace. As a second-order filter, the LC network minimizes the component count. In addition, its small series inductance produces a minimal voltage drop between the input supply and the charge pump.

    Figure 5. Charge-pump inverter with input LC filter.

    Figure 5. Charge-pump inverter with input LC filter.

    The ripple-frequency fundamental equals the pump frequency (FCLOCK/2). Second-order filters attenuate at 40dB/decade, so the ideal filter frequency should be a minimum of one decade below the chosen FCLOCK/2.

    Equation 1

    The inductor must handle dc currents greater than 1.5IOUT without saturation. For critical damping (ie., with no peaking),

    Equation 2

    The filter should be critically damped or close to it, given the low impedance values of RSOURCE and RLOAD. Critical damping is not essential to the circuit operation, however. Filtering remains effective even with some peaking at the point of roll-off. A 10µF filter capacitor and 10µH filter choke together provide a 3dB frequency of 15.9kHz and a critical RSOURCE of 1Ω. Figure 6 shows the Figure 5 circuit's amplitude response for various damping ratios, and Figure 7 shows its lower levels of ripple (vs. the circuit of Figure 3).

    Figure 6. Amplitude characteristic for various damping ratios in the LC-Filter circuit of Figure 5.

    Figure 6. Amplitude characteristic for various damping ratios in the LC-Filter circuit of Figure 5.

    Figure 7. Input voltage and current ripple of LC-filter circuit (Figure 5). CIN = CFILTER = 100µF, and LFILTER = 10µH. Charge pump is MAX665. Input current ripple (upper trace): 100mA/div. Input voltage ripple (lower trace): 50mV/div, AC coupled.

    Figure 7. Input voltage and current ripple of LC-filter circuit (Figure 5). CIN = CFILTER = 100µF, and LFILTER = 10µH. Charge pump is MAX665. Input current ripple (upper trace): 100mA/div. Input voltage ripple (lower trace): 50mV/div, AC coupled.

  3. Adding a low-dropout linear regulator to the charge pump's input supply (Figure 8) yields an effective general-purpose circuit for preventing the effects of ripple on the rest of the system. The input LDO also operates with smaller capacitors than those associated with a passive LC filter: the 300mA MAX8860 LDO (available in an 8-pin µMAX® package) requires 2.2µF capacitors at input and output; the MAX8863MAX8864 family of 120mA linear regulators (available in SOT23 packages) requires only 1µF ceramic capacitors. The LDO must handle at least twice the charge pump's output load current, however. When compared with an equivalent passive filter, the added expense of that extra-current capability can place the LDO approach out of bounds in terms of cost and performance (pcb area and attenuation).

    Figure 8. Charge pump doubler with LDO for input-ripple protection.

    Figure 8. Charge pump doubler with LDO for input-ripple protection.

  4. Adding an RC to the input supply (Figure 9) is a single-order version of the LC-filter approach. The RC input is not generally recommended, because the low value of RFILTER required for minimal efficiency loss (< 5Ω) forces a very large CFILTER. Figure 10 shows the effect of adding an RC filter at the input of the Figure 9 circuit, in which a MAX665 with 100µF capacitors generates a 5V output with a load resistance of 51Ω

    Figure 9. Battery application featuring a charge pump inverter with input RC ripple filter.

    Figure 9. Battery application featuring a charge pump inverter with input RC ripple filter.

    If the input supply is a battery, then the effective bulk capacitance of the battery can serve as CFILTER. Because CFILTER is a very large capacitance, the resulting filter is very effective in reducing ripple effects at the battery. An example helps to illustrate the point: the capacitance of an 800mAH Li cell can be derived from:

    Q = C.V , where I = 800mA, T = 3600s (1Hr), and V = 3.4V.
    I.T = C.V
    Thus, C = 847 farads and fFILTER = 0.12mHz. The sum of ESR and battery contact resistance (about 100mΩ) limits the attenuation to a maximum of 21dB, assuming the ripple source resistance (RFILTER) equals 1Ω. The model for an actual battery is more complex, with the central bulk capacitance modified by ESR, ESL, and parasitic capacitance. In practice one should add capacitance close to RFILTER, thereby providing high frequency assistance and low ESR above 250kHz (< 50mΩ) to the battery and its interconnect leads. A typical value for the additional CFILTER is 470nF. For the MAX665 circuit of Figure 10, increasing CFILTER to 1500µF lowers the input voltage and current ripple as shown in Figure 11.

    Figure 10. Input Voltage and Current Ripple for the RC-filter circuit (Figure 9): CIN = CFILTER = 100µF, and RFILTER = 2.2ohm. Charge pump is a MAX665. Input current ripple (upper trace): 100mA/div. Input voltage ripple (lower trace): 20mV/div, AC coupled.

    Figure 10. Input Voltage and Current Ripple for the RC-filter circuit (Figure 9): CIN = CFILTER = 100µF, and RFILTER = 2.2Ω. Charge pump is a MAX665. Input current ripple (upper trace): 100mA/div. Input voltage ripple (lower trace): 20mV/div, AC coupled.

    Figure 11. Input voltage and current ripple for the RC-filter circuit of Figure 7, with 1500µF quasi-battery capacitor: CIN =100µF, CFILTER = 1500µF, RFILTER = 2.2ohm, and MAX665 charge pump. Input current ripple (upper trace): 100mA/div. Input voltage ripple (lower trace): 20mA/div, AC coupled.

    Figure 11. Input voltage and current ripple for the RC-filter circuit of Figure 7, with 1500µF quasi-battery capacitor: CIN =100µF, CFILTER = 1500µF, RFILTER = 2.2Ω, and MAX665 charge pump. Input current ripple (upper trace): 100mA/div. Input voltage ripple (lower trace): 20mA/div, AC coupled.

Conclusion

Several methods are available for reducing the effect of input power-supply ripple caused by charge pumps. Placing an LC filter in addition to the input capacitor recommended by the data sheet, for instance, (#2) provides excellent voltage-ripple protection to the rest of the system (Figure 10) with minimal effect on the overall conversion efficiency. An effective alternative for battery systems is a simple series resistor (#4), which occupies minimal space. The resistor is also suitable in non-battery applications for which large storage values (> 50µF) are appropriate. Results of a simulated battery application are shown in Figure 11.

An overview of Maxim's charge-pump ICs (Table 1) is included to help the reader choose an appropriate device according to the desired clock frequency, mode of operation, and level of output current required.

Table 1 Product Selection
PartNo MAX660 MAX665 MAX860 MAX861
Package 8-SO 16-wSO 8-µMax/SO 8-µMax/SO
I/P Volts 1.5V to 5.5V 1.5V to 8V 1.5V (inv) or 2.5V to 5.5V 1.5V (inv) or 2.5V to 5.5V
O/P Current 100mA 100mA 50mA 50mA
Pump Rate 10kHz/80kHz 10kHz/45kHz 3kHz/50kHz/130kHz 13kHz/100kHz/250kHz
Mode -VIN, +2VIN -VIN, +2VIN -VIN, +2VIN -VIN, +2VIN
Regulated No No No No
Part No MAX1680 MAX1681 MAX1682 MAX1683
Package 8-SO 8-SO 5-SOT23 5-SOT23
I/P Volts 2.0V to 5.5V 2.0V to 8V 1.5V (inv) or 2.5V to 5.5V 1.5V (inv) or 2.5V to 5.5V
O/P Current 125mA 125mA 45mA 45mA
Clock Freq 125kHz/250kHz 500kHz/1MHz 12kHz 35kHz
Mode -VIN, +2VIN -VIN, +2VIN +2VIN +2VIN
Regulated No No No No
Part No MAX870 MAX871 MAX 1697 R,S,T,U MAX1720
Package 5-SOT23 5-SOT23 6-SOT23 6-SOT23
I/P Volts 1.4V to 5.5V 1.4V to 5.5V 1.5V to 5.5V 1.5V to 5.5V
O/P Current 25mA 25mA 60mA 25mA
Clock Freq 125kHz 500kHz 12kHz/35kHz/125kHz/250kHz 12kHz
Mode -VIN -VIN -VIN -VIN
Regulated No No No No
Part No MAX1719 /MAX1721 MAX864 MAX865 MAX680
Package 6-SOT23 16-QSOP 8-µMax 8-SO
I/P Volts 1.5V to 5.5V 2.0V to 6.0V 1.5V to 6.0V 2.0V to 6.0V
O/P Current 25mA ±10mA ±10mA ±10mA
Clock Freq 125kHz 7kHz/33kHz/100kHz/185kHz 24kHz 8kHz
Mode -VIN +2VIN and -VIN +2VIN and -VIN +2VIN and -VIN
Regulated No No No No
Part No MAX619 MAX622A MAX679 MAX682
Package 8-µMax 8-SO 8-µMax 8-SO
I/P Volts 2.0V to 3.6V 4.5V to 5.5V 1.8V to 3.6V 2.7V to 5.5V
O/P Current 60mA 30mA 20mA 250mA
Clock Freq 500kHz 500kHz 330kHz/1MHz 200kHz/1MHz
Regulated Yes Yes Yes Yes
Part No MAX683 MAX684 MAX768 MAX840/MAX843/MAX844
Package 8-µMax 8-µMax 16-QSOP 8-SO
I/P Volts 2.7V to 5.5V 2.7V to 5.5V 3.0V to 5.5V 2.5V to 10.0V
O/P Current 100mA 50mA ±5mA 4mA
Clock Freq 5.0V 5.0V ±5V, Adj -2.0V, Adj
Mode 200kHz/1MHz 200kHz/1MHz 25kHz/100kHz, 20kHz-240kHz ext sync 20kHz/100kHz
Regulated Yes Yes Yes Yes
Part No MAX850/ MAX851/ MAX852/ MAX853 MAX868 MAX881R MAX1673
Package 8-SO 10-µMax 10-µMax 8-SO
I/P Volts 4.5V to 10.0V 1.8V to 5.5V 2.5V to 5.5V 2.0V to 5.5V
O/P Current 5mA 30mA 4mA 125mA
O/P Volts -4.1V, Adj Adj, -2VIN max -2V, Adj Adj, -VIN max
Clock Freq 100kHz 50kHz-250kHz ext sync 450kHz 100kHz 350kHz
Regulated Yes Yes Yes Yes
Part No MAX1686 /MAX1686H MAX1730 MAX1759  
Package 8-µMax 10-µMax 8-µMax  
I/P Volts 2.7V to 4.2V 2.7V to 5.5V 1.6V to 5.5V  
O/P Current 12mA 50mA 100mA  
O/P Volts 4.75V/5.0V 1.8V/1.9V Adj 3.3V, Adj  
Clock Freq 1MHz 450kHz 1.5MHz  
Regulated Yes Yes Yes  


この記事に関して

製品カテゴリ

最新メディア 21

Subtitle
さらに詳しく
3