要約
This application note provides information on how to interface a DS1307 real-time clock (RTC) to a microcontroller and provides some example code for accessing the part.
Introduction
The DS1307 Serial Real Time Clock, which incorporates a 2-wire serial interface, can be controlled using an 8051-compatible microcontroller. The DS1307 in this example is connected directly to two of the I/O ports on a DS5000 microcontroller and the 2-wire handshaking is handled by low-level drivers, which are discussed in this application note.
DS1307 Description
The DS1307 Serial Real Time Clock is a low-power, full BCD clock/calendar plus 56 bytes of nonvolatile SRAM. Address and data are transferred serially via the 2-wire bi-directional bus. The clock/calendar provides seconds, minutes, hours, day, date, month, and year information. The end of the month date is automatically adjusted for months with less than 31 days, including corrections for leap year. The clock operates in either the 24-hour or 12-hour format with AM/PM indicator. The DS1307 has a built-in power sense circuit which detects power failures and automatically switches to the battery supply.
DS1307 Operation
The DS1307 operates as a slave device on the serial bus. Access is obtained by implementing a START condition and providing a device identification code followed by a register address. Subsequent registers can be accessed sequentially until a STOP condition is executed. The START and STOP conditions are generated using the low level drives, SEND_START and SEND_STOP found in the attached DS5000 code. Also the subroutines SEND_BYTE and READ_BYTE provide the 2-wire handshaking required for writing and reading 8-bit words to and from the DS1307.
Hardware Configuration
The system is configured as shown in Figure 1. The DS1307 has the 2-wire bus connected to two I/O port pins of the DS5000: SCL - P1.0, SDA - P1.1. The VDD voltage is 5V, RP = 5KΩ and the DS5000 is using a 12-MHz crystal. The other peripheral device could be any other device that recognizes the 2-wire protocol, such as the DS1621 Digital Thermometer and Thermostat. The interface with the D5000 was accomplished using the DS5000T Kit hardware and software. This development kit allows the PC to be used as a dumb terminal using the DS5000's serial ports to communicate with the keyboard and monitor.
Figure 1. Typical 2-wire bus configuration.
The following bus protocol has been defined (see Figure 2).
During data transfer, the data line must remain stable whenever the clock line is high. Changes in the data line while the clock line is high will be interpreted as control signals.
Accordingly, the following bus conditions have been defined:
Start data transfer: A change in the state of the data line from high to low, while the clock line is high, defines a START condition.
Stop data transfer: A change in the state of the data line from low to high, while the clock line is high, defines the STOP condition.
Data valid: The state of the data line represents valid data when, after a START condition, the data line is stable for the duration of the high period of the clock signal. The data on the line must be changed during the low period of the clock signal. There is one clock pulse per bit of data.
Each data transfer is initiated with a START condition and terminated with a STOP condition. The number of data bytes transferred between the START and the STOP conditions is not limited, and is determined by the master device. The information is transferred byte-wise and each receiver acknowledges with a ninth bit.
Acknowledge: Each receiving device, when addressed, is obliged to generate an acknowledge after the reception of each byte. The master device must generate an extra clock pulse which is associated with this acknowledge bit.
A device that acknowledges must pull down the SDA line during the acknowledge clock pulse in such a way that the SDA line is stable low during the high period of the acknowledge related clock pulse. Of course, setup and hold times must be taken into account. A master must signal an end of data to the slave by not generating an acknowledge bit on the last byte that has been clocked out of the slave. In this case, the slave must leave the data line high to enable the master to generate the STOP condition.
Figure 2 details how data transfer is accomplished on the 2-wire bus. Depending on the state of the R/active-low W bit, two types of data transfer are possible:
- Data transfer from a master transmitter to a slave receiver. The first byte transmitted by the master is the slave address. Next follows a number of data bytes. The slave returns an acknowledge bit after each received byte. Data is transferred with the most significant bit (MSB) first.
- Data transfer from a slave transmitter to a master receiver. The first byte (the slave address) is transmitted by the master. The slave then returns an acknowledge bit. This is followed by the slave transmitting a number of data bytes. The master returns an acknowledge bit after all received bytes other than the last byte. At the end of the last received byte, a not acknowledge is returned.
Figure 2. Data transfer on 2-wire serial bus.
The master device generates all of the serial clock pulses and the START and STOP conditions. A transfer is ended with a STOP condition or with a repeated START condition. Since a repeated START condition is also the beginning of the next serial transfer, the bus will not be released. Data is transferred with the most significant bit (MSB) first.
The DS1307 may operate in the following two modes:
- Slave receiver mode (DS1307 write mode): Serial data and clock are received through SDA and SCL. After each byte is received, an acknowledge bit is transmitted. START and STOP conditions are recognized as the beginning and end of a serial transfer. Address recognition is performed by hardware after reception of the slave address and direction bit (see Figure 3). The address byte is the first byte received after the start condition is generated by the master. The address byte contains the 7-bit DS1307 address, which is 1101000, followed by the direction bit (R/active-low W) which for a write is a 0. After receiving and decoding the address byte, the DS1307 outputs an acknowledge on the SDA line. After the DS1307 acknowledges the slave address + write bit, the master transmits a register address to the DS1307. This will set the register pointer on the DS1307. The master will then begin transmitting each byte of data with the DS1307 acknowledging each byte received. The master will generate a stop condition to terminate the data write.
Figure 3. Data write—slave receiver mode.
- Slave transmitter mode (DS1307 read mode): The first byte is received and handled as in the slave receiver mode. However, in this mode, the direction bit will indicate that the transfer direction is reversed. Serial data is transmitted on SDA by the DS1307 while the serial clock is input on SCL. START and STOP conditions are recognized as the beginning and end of a serial transfer (See Figure 4). The address byte is the first byte received after the start condition is generated by the master. The address byte contains the 7-bit DS1307 address, which is 1101000, followed by the direction bit (R/active-low W), which for a read is a 1. After receiving and decoding the address byte, the DS1307 inputs an acknowledge on the SDA line. The DS1307 then begins to transmit data starting with the register address pointed to by the register pointer. If the register pointer is not written to before the initiation of a read mode, the first address that is read is the last one stored in the register pointer. The DS1307 must be sent a Not-Acknowledge bit by the master to terminate a read.
Figure 4. Data read—slave transmitter mode.
Software Operation
DS5000 Interface
The software presented in Appendix 1 is written to interface the DS5000 with the DS1307 over the 2-wire interface. The DS5000 was programmed using Dallas Semiconductor's DS5000T Evaluation Kit, which allows a PC to be used as a dumb terminal. The KIT5K software environment supplied with the DS5000T Evaluation Kit provides a high-level interface for loading application software to the DS5000 or for setting its configuration parameters via the Program command. The KIT5K software includes a dumb terminal emulator to allow users to run application software in the DS5000, which communicates with the user via a PC COM port.
DS1307 Source Code
The first section of the code found in the Appendix is used to configure the DS5000 for serial communication with the PC. Also at the beginning of the code is the MASTER_CONTROLLER subroutine which is used to control the demonstration software.
The subroutines that immediately follow the MASTER_CONTROLLER subroutine are the low level drivers for controlling the 2-wire interface. They are not specific to the DS1307 but can be used with any 2-wire compatible slave-only device. These subroutines are:
SEND_START
- This subroutine is used to generate the Start condition on the 2-wire bus.
SEND_STOP
- This subroutine is used to generate the Stop condition on the 2-wire bus.
SEND_BYTE
- This subroutine sends an 8-bit word, MSB first, over the 2-wire bus with a 9th clock pulse for the Acknowledge pulse.
READ_BYTE
- This subroutine reads an 8-bit word over the 2-wire bus. It checks for the LASTREAD flag to be cleared indicating when the last read from the slave device is to occur. If it is not the last read, the DS5000 sends an Acknowledge pulse on the 9th clock and if it is the last read from the slave device, the DS5000 sends a Not-Acknowledge.
SCL_HIGH
- This subroutine transitions the SCL line low-to-high and ensures the SCL line is high before continuing.
DELAY and DELAY_4
- These two subroutines have been included to ensure that the 2-wire bus timing is maintained.
The rest of the code included in the appendix is specifically designed to demonstrate the functions of the DS1307. The functions that are demonstrated are:
Setting Time
- The time is read in from the keyboard and stored in the DS5000 scratchpad memory. It is then transferred, over the 2-wire interface, to the DS1307.
Set RAM
- A single hex byte is read in from the keyboard and written to the entire user RAM of the DS1307.
Read Date/Time
- The date and time are read, over the 2-wire bus, and stored in the DS5000 scratchpad memory. It is then written to the screen. This continues until a key is pressed on the keyboard.
Read RAM
- The entire user RAM of the DS1307 is read into the DS5000 scratchpad memory and then written to the PC monitor.
OSC On/ OSC Off
- The DS1307 clock oscillator can be turned on or off.
SQW/OUT On/ SQW/OUT Off
- The SQW/OUT can be turned on or off. It will toggle at 1 Hz.
Conclusion
It has been shown that it is very straight forward to interface the DS1307 or any other 2-wire slave device to an 8051-compatible microcontroller. The only concern must be that the 2-wire timing specification is not violated by the low level drivers on the microcontroller. The delay subroutines have been inserted into the code for this purpose. The values in Table 1 are the actual timing parameters observed in the hardware setup used to develop this application note.
Parameter | Symbol | Actual | Units |
SCL Clock Frequency | fSCL | 59 | kHz |
Bus Free Time Between a STOP and START condition | tBUF | 5.7 | µs |
Hold Time (repeated) START Condition | tHD:STA | 6.2 | µs |
LOW Period of SCL Clock | tLOW | 10.5 | µs |
HIGH Period of SCL Clock | tHIGH | 6.5M | µs |
Set-up Time for a Repeated START Condition | tSU:STA | 5.3 | µs |
Data Hold Time | tHD:DAT | 5.5 | µs |
Data Set-up Time | tSU:DAT | 3.1 | µs |
Set-up Time for STOP Condition | tSU:STO | 5.4 | µs |
Appendix: DS1307.ASM
; Program DS1307.ASM ; ; This program responds to commands received over the serial ; port to set the date/time as well as RAM data on the DS1307 ; using a DS5000 as a controller ; CR EQU 0DH LF EQU 0AH MCON EQU 0C6H TA EQU 0C7H SCL BIT P0.0 SDA BIT P0.1 TRIG BIT P0.2 DS1307W EQU 0D0H DS1307R EQU 0D1H FLAGS DATA 20H LASTREAD BIT FLAGS.0 _12_24 BIT FLAGS.1 PM_AM BIT FLAGS.2 OSC BIT FLAGS.3 SQW BIT FLAGS.4 ACK BIT FLAGS.5 BUS_FAULT BIT FLAGS.6 _2W_BUSY BIT FLAGS.7 BITCOUNT DATA 21H BYTECOUNT DATA 22H BYTE DATA 23H CSEG AT 0 AJMP START ; CSEG AT 30H ;************************************************************* ;*** RESET GOES HERE TO START PROGRAM **** ;************************************************************* START: MOV TA,#0AAH ; Timed MOV TA,#55H ; access. MOV PCON,#0 ; Reset watchdog timer. MOV MCON,#0F8H ; Turn off CE2 for memory access. MOV SP,#70H ; Position stack above buffer. MOV IE,#0 MOV TMOD,#20H ; Initialize the MOV TH1,#0FAH ; serial port MOV TL1,#0FAH ; for 9600 ORL PCON,#80H ; baud. MOV SCON,#52H MOV TCON,#40H ;MOV R0,#0 ;MOV R1,#0 ;DJNZ R0,$ ;DJNZ R1,$-2 SETB SDA ; ENSURE SDA HIGH LCALL SCL_HIGH ; ENSURE SCL HIGH CLR ACK ; CLEAR STATUS FLAGS CLR BUS_FAULT CLR _2W_BUSY ;----------------------------------------------------------------------- ; THIS IS THE MASTER CONTROLLER LOOP ;----------------------------------------------------------------------- MASTER_CONTROLLER: MOV BYTECOUNT,#10H FORM_FEED: MOV A,#LF ; CLEAR SCREEN FOR MAIN MENU LCALL WRITE_DATA DJNZ BYTECOUNT,FORM_FEED MOV DPTR, #TEXT0 ; PUT MAIN MENU ON SCREEN LCALL WRITE_TEXT MOV DPTR, #TEXT3 LCALL WRITE_TEXT LCALL READ_DATA CLR ACC.5 ; CONVERT ACC TO UPPER CASE CJNE A,#'A',NOTA ; CALL SET CLOCK FUNCTION LCALL SET_CLOCKM JMP MASTER_CONTROLLER ; RETURN TO MAIN MENU NOTA: CJNE A,#'B',NOTB ; CALL SET RAM FUNCTION AND LCALL SET_RAM ; CALL READ RAM FUNCTION LCALL READ_RAM JMP MASTER_CONTROLLER ; RETURN TO MAIN MENU NOTB: CJNE A,#'C',NOTC ; CALL READ CLOCK FUNCTION LCALL READ_CLOCK JMP MASTER_CONTROLLER ; RETURN TO MAIN MENU NOTC: CJNE A,#'D',NOTD ; CALL READ RAM FUNCTION LCALL READ_RAM JMP MASTER_CONTROLLER ; RETURN TO MAIN MENU NOTD: CJNE A,#'E',NOTE ; CALL OSC CONTROL FUNCTION CLR OSC ; CLR OSC FLAG - ON LCALL OSC_CONTROL JMP MASTER_CONTROLLER ; RETURN TO MAIN MENU NOTE: CJNE A,#'F',NOTF ; CALL OSC CONTROL FUNCTION SETB OSC ; SET OSC FLAG - OFF LCALL OSC_CONTROL JMP MASTER_CONTROLLER ; RETURN TO MAIN MENU NOTF: CJNE A,#'G',NOTG ; CALL SWQ CONTROL FUNCTION CLR SQW ; CLR SQW FLAG - ON LCALL SQW_CONTROL_1HZ JMP MASTER_CONTROLLER ; RETURN TO MAIN MENU NOTG: CJNE A,#'H',NOTH ; CALL SWQ CONTROL FUNCTION CLR SQW ; CLR SQW FLAG - ON LCALL SQW_CONTROL_4KHZ JMP MASTER_CONTROLLER ; RETURN TO MAIN MENU NOTH: CJNE A,#'I',NOTI ; CALL SWQ CONTROL FUNCTION CLR SQW ; CLR SQW FLAG - ON LCALL SQW_CONTROL_8KHZ JMP MASTER_CONTROLLER ; RETURN TO MAIN MENU NOTI: CJNE A,#'J',NOTJ ; CALL SWQ CONTROL FUNCTION CLR SQW ; CLR SQW FLAG - ON LCALL SQW_CONTROL_32KHZ JMP MASTER_CONTROLLER ; RETURN TO MAIN MENU NOTJ: CJNE A,#'K',NOTK ; CALL SWQ CONTROL FUNCTION SETB SQW ; SET SQW FLAG - OFF LCALL SQW_CONTROL_1HZ JMP MASTER_CONTROLLER NOTK: CJNE A,#'L',NOTL LCALL SET_RAM_UNQ LCALL READ_RAM NOTL: JMP MASTER_CONTROLLER ; RETURN TO MAIN MENU ;----------------------------------------------------------------------- ; THIS SUB SENDS THE START CONDITION ;----------------------------------------------------------------------- SEND_START: ; SETB _2W_BUSY ; INDICATE THAT 2WIRE OPERATION IN PROGRESS CLR ACK ; CLEAR STATUS FLAGS CLR BUS_FAULT JNB SCL,FAULT ; CHECK FOR BUS CLEAR JNB SDA,FAULT ; BEGIN START CONDITION SETB SDA ; LCALL SCL_HIGH ; SDA CLR SDA ; LCALL DELAY ; SCL ^START CONDITION CLR SCL RET FAULT: SETB BUS_FAULT ; SET FAULT STATUS RET ; AND RETURN ;----------------------------------------------------------------------- ; THIS SUB SENDS THE STOP CONDITION ;----------------------------------------------------------------------- SEND_STOP: ; CLR SDA ; SDA LCALL SCL_HIGH ; SETB SDA ; SCL ^STOP CONDITION CLR _2W_BUSY RET ;----------------------------------------------------------------------- ; THIS SUB SENDS ONE BYTE OF DATA TO THE DS1307 ;----------------------------------------------------------------------- SEND_BYTE: MOV BITCOUNT,#08H ; SET COUNTER FOR 8 BITS SB_LOOP: JNB ACC.7,NOTONE ; CHECK TO SEE IF BIT 7 OF ACC IS A 1 SETB SDA ; SET SDA HIGH (1) JMP ONE NOTONE: CLR SDA ; CLR SDA LOW (0) ONE: LCALL SCL_HIGH ; TRANSITION SCL LOW-TO-HIGH RL A ; ROTATE ACC LEFT ONE BIT CLR SCL ; TRANSITION SCL HIGH-TO-LOW DJNZ BITCOUNT,SB_LOOP ; LOOP FOR 8 BITS SETB SDA ; SET SDA HIGH TO LOOK FOR ACKNOWLEDGE PULSE LCALL SCL_HIGH ; TRASITION SCL LOW-TO-HIGH CLR ACK ; CLEAR ACKNOWLEDGE FLAG JNB SDA,SB_EX ; CHECK FOR ACK OR NOT ACK SETB ACK ; SET ACKNOWLEDGE FLAG FOR NOT ACK SB_EX: LCALL DELAY ; DELAY FOR AN OPERATION CLR SCL ; TRANSITION SCL HIGH-TO-LOW LCALL DELAY ; DELAY FOR AN OPERATION RET ;----------------------------------------------------------------------- ; THIS SUB READS ONE BYTE OF DATA FROM THE DS1307 ;----------------------------------------------------------------------- READ_BYTE: MOV BITCOUNT,#008H ; SET COUNTER FOR 8 BITS OF DATA MOV A,#00H ; SETB SDA ; SET SDA HIGH TO ENSURE LINE FREE READ_BITS: LCALL SCL_HIGH ; TRANSITION SCL LOW-TO-HIGH MOV C,SDA ; MOVE DATA BIT INTO CARRY BIT RLC A ; ROTATE CARRY BIT INTO ACC.0 CLR SCL ; TRANSITION SCL HIGH-TO-LOW DJNZ BITCOUNT,READ_BITS ; LOOP FOR 8 BITS JB LASTREAD,ACKN ; CHECK TO SEE IF THIS IS THE LAST READ CLR SDA ; IF NOT LAST READ SEND ACKNOWLEDGE BIT ACKN: LCALL SCL_HIGH ; PULSE SCL TO TRANSIMIT ACKNOWLEDGE CLR SCL ; OR NOT ACKNOWLEDGE BIT RET ;----------------------------------------------------------------------- ; ; THIS SUB SETS THE CLOCK LINE HIGH ;----------------------------------------------------------------------- SCL_HIGH: SETB SCL ; SET SCL HIGH JNB SCL,$ ; LOOP UNTIL STRONG 1 ON SCL RET ;----------------------------------------------------------------------- ; ; THIS SUB DELAY THE BUS ;----------------------------------------------------------------------- DELAY: NOP ; DELAY FOR BUS TIMING RET ;----------------------------------------------------------------------- ; THIS SUB DELAYS 4 CYCLES ;----------------------------------------------------------------------- DELAY_4: NOP ; DELAY FOR BUS TIMING NOP NOP NOP RET ;----------------------------------------------------------------------- ; THIS SUB SETS THE CLOCK (MANUAL) ;----------------------------------------------------------------------- SET_CLOCKM: MOV R1,#2EH ; SET R1 TO SCRATCHPAD MEMORY FOR DATE/TIME MOV DPTR, #YEAR ; GET THE DATE/TIME INFORMATION FROM THE LCALL WRITE_TEXT ; USER. WRITE THE DATE/TIME TO SCRATCHPAD LCALL READ_BCD ; MEMORY MOV @R1,A DEC R1 MOV DPTR, #MONTH LCALL WRITE_TEXT LCALL READ_BCD MOV @R1,A DEC R1 MOV DPTR, #DAY LCALL WRITE_TEXT LCALL READ_BCD MOV @R1,A DEC R1 MOV DPTR, #DAYW LCALL WRITE_TEXT LCALL READ_BCD ANL A, #7 MOV @R1,A DEC R1 MOV DPTR, #HOUR LCALL WRITE_TEXT LCALL READ_BCD MOV @R1,A DEC R1 MOV DPTR, #MINUTE LCALL WRITE_TEXT LCALL READ_BCD MOV @R1,A DEC R1 MOV DPTR, #SECOND LCALL WRITE_TEXT LCALL READ_BCD MOV @R1,A MOV R1,#28H ; POINT TO BEGINNING OF CLOCK DATA IN SCRATCHPAD MEMORY LCALL SEND_START ; SEND 2WIRE START CONDITION MOV A,#DS1307W ; SEND DS1307 WRITE COMMAND LCALL SEND_BYTE MOV A,#00H ; SET DATA POINTER TO REGISTER 00H ON LCALL SEND_BYTE ; THE DS1307 SEND_LOOP: MOV A,@R1 ; MOVE THE FIRST BYTE OF DATA TO ACC LCALL SEND_BYTE ; SEND DATA ON 2WIRE BUT INC R1 CJNE R1,#2FH,SEND_LOOP ; LOOP UNTIL CLOCK DATA SENT TO DS1307 LCALL SEND_STOP ; SEND 2WIRE STOP CONDITION RET ;----------------------------------------------------------------------- ; THIS SUB SETS THE DS1307 USER RAM TO THE VALUE IN 'BYTE' ;----------------------------------------------------------------------- SET_RAM: MOV R1,#08H ; POINTER TO BEGINNING OF DS1307 USER RAM MOV DPTR, #TEXT5 ; MESSAGE TO ENTER DATA BYTE LCALL WRITE_TEXT ; LCALL READ_BCD ; READ BYTE FROM KEYBOARD MOV BYTE,A ; AND STORE IN 'BYTE' LCALL SEND_START ; SEND 2WIRE START CONDITION MOV A,#DS1307W ; LOAD DS1307 WRITE COMMAND LCALL SEND_BYTE ; SEND WRITE COMMAND MOV A,#08H ; SET DS1307 DATA POINTER TO BEGINNING LCALL SEND_BYTE ; OF USER RAM - 08H SEND_LOOP2: MOV A,BYTE ; WRITE BYTE TO ENTIRE RAM SPACE LCALL SEND_BYTE ; WHICH IS 08H TO 37H INC R1 CJNE R1,#040H,SEND_LOOP2 ; LOOP UNTIL RAM FILLED LCALL SEND_STOP ; SEND 2WIRE STOP CONTION RET ;----------------------------------------------------------------------- ; THIS SUB SETS THE DS1307 USER RAM TO THE UNIQUE PATTERN ;----------------------------------------------------------------------- SET_RAM_UNQ: MOV R1,#08H ; POINTER TO BEGINNING OF DS1307 USER RAM LCALL SEND_START ; SEND 2WIRE START CONDITION MOV A,#DS1307W ; LOAD DS1307 WRITE COMMAND LCALL SEND_BYTE ; SEND WRITE COMMAND MOV A,#08H ; SET DS1307 DATA POINTER TO BEGINNING LCALL SEND_BYTE ; OF USER RAM - 08H SEND_LOOP3: LCALL SEND_BYTE ; WHICH IS 08H TO 37H INC R1 INC A CJNE R1,#040H,SEND_LOOP3 ; LOOP UNTIL RAM FILLED LCALL SEND_STOP ; SEND 2WIRE STOP CONTION RET ;----------------------------------------------------------------------- ; THIS SUB READS THE DS1307 RAM AND WRITES IT TO THE SCRATCH PAD MEMORY ;----------------------------------------------------------------------- READ_RAM: MOV DPTR,#TEXT4 ; SEND KEY PRESS MSG LCALL WRITE_TEXT MOV R1,#30H ; START OF RAM REGS IN SCRATCH PAD MOV BYTECOUNT,#00H ; COUNTER FOR 56 RAM BYTES CLR LASTREAD ; FLAG TO CHECK FOR LAST READ LCALL SEND_START ; SEND 2WIRE START CONDITION MOV A,#DS1307W ; SEND DS1307 WRITE COMMAND LCALL SEND_BYTE MOV A,#08H ; SET POINTER TO REG 08H ON ;DS1307 LCALL SEND_BYTE LCALL SEND_STOP ; SEND STOP CONDITION LCALL SEND_START ; SEND START CONDITION MOV A,#DS1307R ; SEND DS1307 READ COMMAND LCALL SEND_BYTE READ_LOOP2: MOV A,BYTECOUNT ; CHECK TO SEE OF DOING LAST READ CJNE A,#37H,NOT_LAST2 SETB LASTREAD ; IF LAST READ SET LASTREAD FLAG NOT_LAST2: LCALL READ_BYTE ; READ A BYTE OF DATA MOV @R1,A ; MOVE DATA INTO SCRATCHPAD MEMORY INC R1 ; INC POINTERS INC BYTECOUNT MOV A,BYTECOUNT CJNE A,#38H,READ_LOOP2 ; LOOP FOR ENTIRE DS1307 RAM LCALL SEND_STOP ; SEND 2WIRE STOP CONDITION LCALL DISP_RAM ; DISPLAY DATA IN SCRATCHPAD MEMORY JNB RI,$ ;WAIT UNTIL A KEY IS PRESSED CLR RI RET ;----------------------------------------------------------------------- ; THIS SUB DISPLAYS THE RAM DATA SAVED IN SCRATCHPAD MEMORY ;----------------------------------------------------------------------- DISP_RAM: MOV R1,#30H ;START OF RAM IN SCRATCHPAD ;MEMORY MOV BITCOUNT,#00H MOV DPTR,#TEXT6 ;DISPLAY TABLE HEADING LCALL WRITE_TEXT DISP_ADDR: LCALL DISP_LOC ; DISPLAY VALUE OF CURRENT RAM LOCATION DIS_LOOP: MOV A,@R1 ; DISPLAY RAM DATA SAVED IN SCRATCHPAD LCALL WRITE_BCD ; CONVERT TO BCD FORMAT AND DISPLAY INC R1 INC BITCOUNT MOV A,#20H ; SPACE BETWEEN DATA BYTES LCALL WRITE_DATA MOV A,BITCOUNT CJNE A,#08H,DIS_LOOP ; LINE FEED AFTER 8 BYTES OF DATA MOV BITCOUNT,#00H MOV DPTR,#TEXT3 ; 'CR,LF' LCALL WRITE_TEXT CJNE R1,#68H,DISP_ADDR ; DISPLAY DATA FOR 56 BYTES OF RAM RET ;----------------------------------------------------------------------- ; ; THIS SUB WRITES THE RAM LOCATION OF THE DATA ;----------------------------------------------------------------------- DISP_LOC: MOV A,R1 ; DISPLAY THE HEX VALUE FOR THE DATA ADD A,#-28H ; IN THE DS1307 RAM SPACE LCALL WRITE_BCD ; CONVERTS SCRATCHPAD ADDRESS MOV A,#20H ; INTO DS1307 RAM ADDRESS LCALL WRITE_DATA MOV A,#20H LCALL WRITE_DATA MOV A,#20H LCALL WRITE_DATA RET ;----------------------------------------------------------------------- ; THIS SUB READS THE CLOCK AND WRITES IT TO THE SCRATCH PAD MEMORY ; ;----------------------------------------------------------------------- READ_CLOCK: MOV DPTR,#TEXT4 ; KEY PRESS MSG LCALL WRITE_TEXT READ_AGAIN: MOV R1,#28H ; START OF CLOCK REG IN SCRATCHPAD MOV BYTECOUNT,#00H ; COUNTER UP TO 8 BYTES FOR CLOCK CLR LASTREAD ; FLAG TO CHECK FOR LAST READ LCALL SEND_START ; SEND START CONDITION MOV A,#DS1307W ; SET POINTER TO REG 00H ON DS1307 LCALL SEND_BYTE MOV A,#00H LCALL SEND_BYTE LCALL SEND_STOP ; SEND STOP CONDITION LCALL SEND_START ; SEND START CONDITION MOV A,#DS1307R ; SEND READ COMMAND TO DS1307 LCALL SEND_BYTE READ_LOOP: MOV A,BYTECOUNT ; CHECK TO SEE OF DOING LAST READ CJNE A,#07H,NOT_LAST SETB LASTREAD ; SET LASTREAD FLAG NOT_LAST: LCALL READ_BYTE ; READ A BYTE OF DATA MOV @R1,A ; MOVE DATA IN SCRATCHPAD MEMORY MOV A,BYTECOUNT ; CHECK TO SEE IF READING SECONDS REG CJNE A,#00H,NOT_FIRST CLR OSC ; CLR OSC FLAG MOV A,@R1 ; MOVE SECONDS REG INTO ACC JNB ACC.7,NO_OSC ; JUMP IF BIT 7 OF IS A 0 SETB OSC ; SET OSC FLAG, BIT 7 IS A 1 CLR ACC.7 ; CLEAR BIT 7 FOR DISPLAY ; PURPOSES MOV @R1,A ; MOVE DATA BACK TO SCRATCHPAD NO_OSC: NOT_FIRST: INC R1 ; INC COUNTERS INC BYTECOUNT MOV A,BYTECOUNT CJNE A,#08H,READ_LOOP ; LOOP FOR ENTIRE CLOCK REGISTERS LCALL SEND_STOP ; SEND 2WIRE STOP CONDITION LCALL DISP_CLOCK ; DISPLAY DATE/TIME FROM SCRATCHPAD JNB RI,READ_AGAIN ; READ AND DISPLAY UNTIL A KEY IS PRESSED CLR RI RET ;----------------------------------------------------------------------- ; THIS SUB DISPLAYS THE DATE AND TIME SAVED IN SCRATCHPAD MEMORY ;----------------------------------------------------------------------- DISP_CLOCK: MOV DPTR,#TEXT1 ; DATE: LCALL WRITE_TEXT MOV R1,#2DH ; MONTH MOV A,@R1 LCALL WRITE_BCD MOV A,#'/' LCALL WRITE_DATA MOV R1,#2CH ; DATE MOV A,@R1 LCALL WRITE_BCD MOV A,#'/' LCALL WRITE_DATA MOV R1,#2EH ; YEAR MOV A,@R1 LCALL WRITE_BCD MOV A,#09H ; TAB LCALL WRITE_DATA MOV DPTR,#TEXT2 ; TIME: LCALL WRITE_TEXT MOV R1,#2AH ; HOURS MOV A,@R1 LCALL WRITE_BCD MOV A,#3AH ; COLON LCALL WRITE_DATA MOV R1,#29H ; MINUTES MOV A,@R1 LCALL WRITE_BCD MOV A,#3AH ; COLON LCALL WRITE_DATA MOV R1,#28H ; SECONDS MOV A,@R1 LCALL WRITE_BCD RET ;----------------------------------------------------------------------- ; THIS SUB SETS THE OSCILLATOR ACCORDING TO THE OSC BIT ;----------------------------------------------------------------------- OSC_CONTROL: LCALL SEND_START ; SEND START CONDITION MOV A,#DS1307W ; SET POINTER TO REG 00H ON DS1307 LCALL SEND_BYTE MOV A,#00H LCALL SEND_BYTE SETB LASTREAD ; SET LAST READ FOR SINGLE READ LCALL SEND_STOP ; SEND STOP CONDITION LCALL SEND_START ; SEND START CONDITION MOV A,#DS1307R ; SEND READ COMMAND TO DS1307 LCALL SEND_BYTE LCALL READ_BYTE ; READ SECONDS REGISTER CLR ACC.7 ; TURN OSC ON JNB OSC,OSC_SET SETB ACC.7 ; TURN OSC OFF IF OSC BIT IS SET IN OSC_SET: ; SECONDS REGISTER PUSH ACC ; SAVE SECONDS DATA ON STACK LCALL SEND_STOP ; SEND STOP CONDITION LCALL SEND_START ; SEND START CONDITION MOV A,#DS1307W ; SET POINTER TO REG 00H ON DS1307 LCALL SEND_BYTE MOV A,#00H LCALL SEND_BYTE POP ACC ; SEND SECONDS REGISTER TO CONTROL LCALL SEND_BYTE ; OSCILLATOR ON DS1307 LCALL SEND_STOP RET ;----------------------------------------------------------------------- ; THIS SUB CONTROLS THE SQW OUTPUT 1HZ ;----------------------------------------------------------------------- SQW_CONTROL_1HZ: LCALL SEND_START ; SEND START CONDITION MOV A,#DS1307W ; SET POINTER TO REG 07H ON DS1307 LCALL SEND_BYTE MOV A,#07H LCALL SEND_BYTE MOV A,#90H ; SQW/OUT ON AT 1HZ JNB SQW,SQW_SET ; JUMP IF SQW BIT IS ACTIVE MOV A,#80H ; TURN SQW/OUT OFF - OFF HIGH SQW_SET: LCALL SEND_BYTE LCALL SEND_STOP RET ;----------------------------------------------------------------------- ; THIS SUB CONTROLS THE SQW OUTPUT 4KHZ ;----------------------------------------------------------------------- SQW_CONTROL_4KHZ: LCALL SEND_START ; SEND START CONDITION MOV A,#DS1307W ; SET POINTER TO REG 07H ON DS1307 LCALL SEND_BYTE MOV A,#07H LCALL SEND_BYTE MOV A,#91H ; SQW/OUT ON AT 1HZ JNB SQW,SQW_SET1 ; JUMP IF SQW BIT IS ACTIVE MOV A,#80H ; TURN SQW/OUT OFF - OFF HIGH SQW_SET1: LCALL SEND_BYTE LCALL SEND_STOP RET ;----------------------------------------------------------------------- ; THIS SUB CONTROLS THE SQW OUTPUT 8KHZ ;----------------------------------------------------------------------- SQW_CONTROL_8KHZ: LCALL SEND_START ; SEND START CONDITION MOV A,#DS1307W ; SET POINTER TO REG 07H ON DS1307 LCALL SEND_BYTE MOV A,#07H LCALL SEND_BYTE MOV A,#92H ; SQW/OUT ON AT 1HZ JNB SQW,SQW_SET2 ; JUMP IF SQW BIT IS ACTIVE MOV A,#80H ; TURN SQW/OUT OFF - OFF HIGH SQW_SET2: LCALL SEND_BYTE LCALL SEND_STOP RET ;----------------------------------------------------------------------- ; THIS SUB CONTROLS THE SQW OUTPUT 32KHZ ;----------------------------------------------------------------------- SQW_CONTROL_32KHZ: LCALL SEND_START ; SEND START CONDITION MOV A,#DS1307W ; SET POINTER TO REG 07H ON DS1307 LCALL SEND_BYTE MOV A,#07H LCALL SEND_BYTE MOV A,#93H ; SQW/OUT ON AT 1HZ JNB SQW,SQW_SET3 ; JUMP IF SQW BIT IS ACTIVE MOV A,#80H ; TURN SQW/OUT OFF - OFF HIGH SQW_SET3: LCALL SEND_BYTE LCALL SEND_STOP RET ;----------------------------------------------------------------------- ; THIS SUB IS A SCOPE TRIGGER BIT ;----------------------------------------------------------------------- TRIGGER: CLR TRIG SETB TRIG LCALL DELAY_4 CLR TRIG RET ;----------------------------------------------------------------------- ; THIS SUB READS DATA FROM THE SCREEN AND CONVERTS IT TO BCD FORM ; DATA SHOULD BE HEX DIGITS: 1,2,3...9,A,B,C,D,E,F ;----------------------------------------------------------------------- READ_BCD: MOV R0,#0 ; CLEAR R0 BCD_LOOP: LCALL READ_DATA ; READ BYTE FROM KEYBOARD LCALL WRITE_DATA ; WRITE BYTE BACK TO SCREEN CJNE A, #0DH, BCD ; CHECK FOR CR MOV A,R0 ; MOVE R0 TO ACC AND RETURN RET BCD: ADD A,#-30H ; BEGIN TO CONVERT TO ACTUAL VALUE JNB ACC.4,DIGIT ; JUMP IF NOT A-F ADD A,#-07H ; IF A-F SUBTRACT 7 DIGIT: ANL A,#0FH ; ENSURE BITS 4-7 ARE CLEARED ANL 0,#0FH ; ENSURE BITS 4-7 ARE CLEARED XCH A,R0 ; EXCHANGE R0 AND ACC SWAP A ; NIBBLE SWAP ACC ORL A,R0 ; INSERT BITS 0-3 OF R0 INTO ACC MOV R0,A ; MOVE ACC INTO R0 SJMP BCD_LOOP ; LOOP UNTIL CR ENCOUNTERED ;----------------------------------------------------------------------- ; THIS SUB WRITES THE BYTE TO THE SCREEN ;----------------------------------------------------------------------- WRITE_BCD: PUSH ACC ; SAVE ACC ON STACK SWAP A ; NIBBLE SWAP ACC ANL A,#0FH ; CLEAR BITS 4-7 OF ACC ADD A,#07H ; ADD 7 TO ACC TO CONVERT TO ASCII HEX JNB ACC.4,LESSNINE ; CHECK TO SEE IF LESS THAN NINE 0-8 CJNE A,#10H,NOTNINE ; JUMP IS GREATER THAN NINE A-F LESSNINE: ADD A,#-07H ; SUBTRACT 7 FOR 0-9 NOTNINE: ADD A,#30H ; ADD 30 TO CONVERT TO ASCII EQUIVALENT LCALL WRITE_DATA ; WRITE BYTE TO SCREEN POP ACC ; RECALL ACC FROM STACK ANL A,#0FH ; PERFORM CONVERSION ON OTHER HALF OF BYTE ADD A,#07H JNB ACC.4,NINE2 CJNE A,#10H,NOTNINE2 NINE2: ADD A,#-07H NOTNINE2: ADD A,#30H LCALL WRITE_DATA RET ;----------------------------------------------------------------------- READ_DATA: JNB RI,READ_DATA ; LOOP WHILE RI BIT IS LOW CLR RI ; MOV A,SBUF ; GET DATA BYTE FROM SERIAL BUFFER RET ;----------------------------------------------------------------------- WRITE_DATA: JNB TI,WRITE_DATA ; LOOP WHILE TI BIT IS LOW CLR TI ; MOV SBUF,A ; SEND DATA BYTE TO SERIAL ; BUFFER RET ;----------------------------------------------------------------------- WRITE_TEXT: PUSH ACC ; SAVE ACC BYTE ON STACK WT1: CLR A ; CLEAR ACC MOVC A,@A+DPTR ; MOVE FIRST BYTE OF STRING ; TO ACC INC DPTR ; INC DATA POINTER CJNE A,#0,WT2 ; CHECK FOR STRING ; TERMINATOR - 0 POP ACC ; RESTORE ACC RET ; RETURN WHEN STRING IS SENT WT2: LCALL WRITE_DATA ; SEND BYTE OF STRING OVER SERIAL PORT SJMP WT1 ;----------------------------------------------------------------------- ; TEXT STRINGS USED FOR USER INTERFACE OVER SERIAL PORT ;----------------------------------------------------------------------- YEAR: DB CR,LF,'YEAR (0 - 99) : ',0 MONTH: DB CR,LF,'MONTH (1 - 12) : ',0 DAY: DB CR,LF,'DAY OF MONTH : ',0 DAYW: DB CR,LF,'DAY OF WEEK : ',0 HOUR: DB CR,LF,'HOUR (0 - 23) : ',0 MINUTE: DB CR,LF,'MINUTE (0 - 59) : ',0 SECOND: DB CR,LF,'SECOND (0 - 59) : ',0 TRIER: DB CR,LF,'PRESS ANY KEY TO SET THIS TIME ',CR,LF,0 TEXT0: DB CR,LF,'******* DALLAS SEMICONDUCTOR ******* ' DB CR,LF,' DS1307 TEST PROGRAM ',CR,LF DB CR,LF,'PLEASE CHOOSE AN OPTION TO CONTINUE ' DB CR,LF,'------------------------------------ ' DB CR,LF,'A. SET TIME(MANUAL) B. SET RAM ' DB CR,LF,'C. READ DATE/TIME D. READ RAM ' DB CR,LF,'E. OSC ON F. OSC OFF ' DB CR,LF DB CR,LF,'G. SQW/OUT ON-1HZ H. SQW/OUT ON-4KHZ' DB CR,LF,'I. SQW/OUT ON-8KHZ J. SQW/OUT ON-32KHZ' DB CR,LF DB CR,LF,'K. SQW/OUT OFF' DB CR,LF,'L. WRITE RAM UNIQUE PATTERN ' DB CR,LF,'ESC. TO QUIT ',0 TEXT1: DB CR,'DATE: ',0 TEXT2: DB 'TIME: ',0 TEXT3: DB CR,LF,0 TEXT4: DB CR,LF,'PRESS ANY KEY TO RETURN' DB CR,LF,0 TEXT5: DB CR,LF,'ENTER THE BYTE VALUE WHICH WILL FILL THE RAM' DB CR,LF,0 TEXT6: DB CR,LF,'RAM RAM' DB CR,LF,'ADDR DATA' DB CR,LF,'-----------------------------' DB CR,LF,0 ;****************************************** ;**** END OF PROGRAM ************ ;****************************************** END