Design Note 50: High Frequency Amplifier Evaluation Board
Introduction
Demo board DC009 is designed to simplify the evaluation of high speed operational amplifiers. It includes both an inverting and non-inverting circuit, and pads are provided to allow the use of board-mounted BNC or SMA connectors. The two circuits are independent, with the exception of shared power supply and ground connections.
High Speed Layout Techniques
Layout is a primary contributor to the performance of any high speed amplifier. Poor layout techniques adversely affect the behavior of a finished circuit. Several important layout techniques, all used in demo board DC009, are described below:
Top Side Ground Plane: The primary task of a ground plane is to lower the impedance of ground connections. The inductance between any two points on a uniform sheet of copper is less than the inductance of a narrow, straight trace of copper connecting the same two points. The ground plane approximates the characteristics of a copper sheet and lowers the impedance at key points in the circuit, such as at the grounds of connectors and supply bypass capacitors.
Ground Plane Voids: Certain components and circuit nodes are very sensitive to stray capacitance. Two good examples are the summing node of the op amp and the feedback resistor. Voids are put in the ground plane in these areas to reduce stray ground capacitance
Input/Output Matching: The width of the input and output traces is adjusted to a stripline impedance of 50Ω. Note that the terminating resistors (R3 and R7) are connected to the end of the input lines — not at the connector. While stripline techniques aren’t absolutely necessary for the demo board, they are important on larger layouts where line lengths are longer. The short lines on the demo board can be terminated in 50Ω, 75Ω, or 93Ω without adversely affecting performance.
Separation of Input and Output Grounds: Even though the ground plane exhibits a low impedance, input and output grounds are still separated. For example, the termination resistors (R3 and R7) and the gain-setting resistor (R1) are grounded in the vicinity of the input connector. Supply bypass capacitors (C1, C2, C4, C5, C7, C8, C9, and C10) are returned to ground in the vicinity of the output connectors.
Figure 1. Demo DC009 High Frequency Amplifier.
Optional Components
The circuit board is designed to accommodate standard 8- pin miniDIP, single operational amplifiers, such as the LT1190 and LT1220 families. Both voltage and current feedback types can be used. Pins 1, 5, and 8 are outfitted with pads for use in adjusting DC offsets, compensation or, in the case of the LT1223 and LT1190/1/2, for shutting down the amplifier.
If a current feedback amplifier such as the LT1223 is being evaluated, omit C3/C6. R4 and R8 are included for impedance matching when driving low impedance lines. If the amplifier is supposed to drive the line directly, or if the load impedance is high, R4 and R8 can be replaced by jumpers. Similarly R10 and R12 can be used to establish a load at the output of the amplifier.
Low profile sockets may be used for the op amps to facilitate changing parts, but performance may be affected above 100MHz.
Supply Bypass Capacitors
High speed operational amplifiers work best when their supply pins are bypassed with RF-quality capacitors. C1, C5, C8, and C10 should be 10nF disc ceramics with a self-resonant frequency greater than 10MHz. The polarized capacitors (C2, C4, C7, and C9) should be 1µF to 10µF tantalums. Most 10nF ceramics are self-resonant well above 10MHz, and 4.7µF solid tantalums (axial leaded) are self-resonant at 1MHz or below. Lead lengths are critical: the self-resonant frequency of a 4.7µF tantalum drops by a factor of 2 when measured through 2 inch leads. Although a capacitor may become inductive at high frequencies, it is still an effective bypass component above resonance because the impedance is low.
Demo Board DC009 Parts List
Non-inverting Amplifier:
R1 Gain Setting Resistor
R2 Feedback Resistor
R3 Input Line Termination (51Ω)
R4 Output Line Termination (51Ω)
R9 Shutdown Pin Pull Down
R10 Output Load Resistor
C1 Positive Supply High Frequency Bypass (10nF)
C2 Positive Supply Low Frequency Bypass (4.7µF)
C3 Feedback Capacitor
C4 Negative Supply Low Frequency Bypass (4.7µF)
C5 Negative Supply High Frequency Bypass (10nF)
C11 Compensation Capacitor
J1 Input Connector (AMP 227699-3)
J2 Output Connector (AMP 227699-3)
Inverting Amplifier:
R5 Feedback Resistor
R6 Gain Setting Resistor
R7 Input Line Termination (51Ω)
R8 Output Line Termination (51Ω)
R1 Shutdown Pin Pull Down
R12 Output Load Resistor
C6 Feedback Capacitor
C7 Positive Supply Low Frequency Bypass (4.7µF)
C8 Positive Supply High Frequency Bypass (10nF)
C9 Negative Supply Low Frequency Bypass (4.7µF)
C10 Negative Supply High Frequency Bypass (10nF)
C12 Compensation Capacitor
J3 Input Connector (AMP 227699-3)
J4 Output Connector (AMP 227699-3)

Figure 2. High Frequency Amplifier, Demo 009A Component Side.