Switch Mode Power Supply Current Sensing - Part 2: Where to Place the Sense Resistor
Switch Mode Power Supply Current Sensing - Part 2: Where to Place the Sense Resistor
Nov 21 2016
Where to Place the Current Sense Resistor
The placement of the current sense resistor in conjunction with the switching regulator architecture determines what current is being sensed. Currents that are sensed include the peak inductor current, the valley inductor current (the minimum value of the inductor current when in continuous conduction mode) and the average output current. The location of the sense resistor affects power loss, noise calculations and the common mode voltage seen by the sense resistor monitoring circuitry.
Buck Regulator High Side Placement
For a step-down (buck) regulator, the current sense resistor can be placed in several locations. When placed on the high side of the top MOSFET (as shown in Figure 1), it detects the peak inductor current when the top MOSFET is on and thus can be used for peak current mode controlled supplies. However, it does not measure inductor current when the top MOSFET is off and the bottom MOSFET is on.

Figure 1. Buck Converter with High Side RSENSE
In this configuration, current sensing can be noisy, because the turn-on edge of the top MOSFET has strong switching voltage ringing. To minimize this affect, a long current comparator blanking time (the time during which the comparator ignores the input) is needed. This limits the minimum switch ON time and can limit the minimum duty cycle (duty cycle= VOUT / VIN) and maximum converter step-down ratio. Note in the high side configuration, the current signal can be riding on top of a very large common mode voltage (VIN).
Buck Regulator Low Side Placement
In Figure 2, the sense resistor is placed below the bottom MOSFET. In this configuration it detects the valley mode current. To further reduce power loss and save component cost, the bottom FET RDS(ON) can be used to sense current without using an external current sensing resistor RSENSE.

Figure 2. Buck Converter with Low Side RSENSE
This configuration is usually used for a valley mode controlled power supply. It can also be sensitive to noise, but in this case it is when the duty cycle is large. A valley mode controlled buck converter allows high step-down ratios; however, its maximum duty-cycle is limited due to its fixed/controlled switch ON time.
Buck Regulator Placement in Series with the Inductor
In Figure 3, the current sensing resistor RSENSE is placed in series with the inductor, so it can detect the continuous inductor current, which can be used for average current monitoring, and peak or valley current monitoring. Accordingly, this configuration allows peak, valley or average current mode controls.

Figure 3. RSENSE in Series with the Inductor
This sensing method provides the best signal-to-noise ratio performance. An external RSENSE usually can provide a very accurate current sensing signal for accurate current limit and sharing. However, the RSENSE also causes additional power loss and component cost. To reduce the power loss and cost, the inductor winding DC resistance (DCR) can be used to sense current without an external RSENSE.
Boost and Inverting Regulators High Side Placement
For a step-up (Boost) regulator, the sense resistor can be placed in series with the inductor providing high side sensing (Figure 4).

Figure 4. Boost Converter with High Side RSENSE
Since the boost has continuous input current, a triangular waveform results and current is continuously monitored.
Boost and Inverting Regulators Low Side Placement
The sense resistor can also be placed on the low side of the bottom MOSFET as shown in Figure 5. Here, the peak switch current (which is also the peak inductor current) is monitored, resulting in a current waveform every half cycle. Due to the MOSFET switching, the current signal has strong switching noises.

Figure 5. Boost Converter with Low Side RSENSE
Buck-Boost Low Side SENSE Resistor Placment or in Series with the Inductor
A 4-switch buck-boost converter is shown below in Figure 6 with the sense resistor on the low side. The converter operates in buck mode when the input voltage is much higher than the output voltage, and in boost mode when the input voltage is much lower than the output voltage. In this circuit, the sense resistor is located at the bottom of the 4-switch H-bridge configuration. The mode of the device (buck mode or boost mode) determines what current is being monitored.

Figure 6. Buck-Boost with RSENSE on the Low Side
In buck mode (switch D always on, switch C always off), the sense resistor monitors the bottom side switch B current and the supply operates as a valley current mode buck converter.
In boost mode (switch A always on, switch B always off) the sense resistor is in series with the bottom MOSFET (C) and measures peak current as the inductor current rises. In this mode, since the valley inductor current is not monitored, it is difficult to detect the negative inductor current when the supply is in light load condition. Negative inductor current means energy is simply being transferred from the output back to the input, but due to losses associated with the transfer, efficiency suffers. So for applications such as battery-powered systems for which light load efficiency is important, this current sensing method is undesirable.
The circuit of Figure 7 resolves this issue by placing the sense resistor in series with the inductor so that the inductor current signal is continually measured in both buck and boost modes. Since current sensing RSENSE is connected to the SW1 node which has high switching noises, the controller IC needs to be carefully designed to allow sufficient blanking time for the internal current comparator.

Figure 7. LT8390 Buck-Boost with RSENSE in series with the Inductor
An additional sense resistor can also be added at the input for input current limiting or at the output (as shown below) for constant output current applications such as battery charging or driving LEDs. In this case, since the average input or output current signal is needed, a strong R/C filter can be added to the current sensing path to reduce current sensing noise.
In most of the above examples, the current sensing element is assumed to be a sense resistor. However, this does not have to be and often is not the case. Other sensing techniques include using the voltage drop across a MOSFET or the DC resistance (DCR) of the inductor. These current sensing methods are addressed in Part 3 "Current Sensing Methods".
About The Authors
Kevin Scott works as a Product Marketing Manager for the Power Products Group at Analog Devices, where he manages Boost, Buck-Boost and Isolated Converters, LED Drivers and Linear Regulators. He previously worked as a Seni...
Henry Zhang is ADI’s Power by Linear™ applications director. He received a B.S.E.E. degree from Zhejiang University, China in 1994 and his M.S. and Ph.D. degrees in electrical engineering from Virginia Polytechnic Institut...
Author's Contact Information