LTspice: Annotating Schematic & Waveform Plots

Sep 4 2013

Adding informative comments to a schematic using text is very useful. However, there are times when adding a line, rectangle, circle or arc to a schematic can better illustrate a circuit. A classic example is highlighting a transformer core using two lines. In LTspice these graphical annotations are available under Draw in the Edit menu. If you do not want these graphical annotations to snap to the grid, you can hold down the Ctrl key while positioning.

Waveform plots can be annotated with text, arrows, lines, boxes and circles. These annotations are effective for illustrating a particular result in your plot to a colleague. Plot annotations along with Move and Drag can be found under Notes & Annotations under Plot Setting menu. Note that if you annotate a plot you will need to save your annotations via a Plot Setting file (available under Plot Setting menu); otherwise they will not be saved.

About The Authors

Gabino Alonso
Gabino Alonso is currently the director of strategic marketing for the Power by Linear™ Group. Prior to joining ADI, Gabino held various positions in marketing, engineering, operations, and education at Linear Technology, ...
Add to myAnalog

Author's Contact Information

Gabino Alonso

Director, Power Strategic Marketing

Related to this Article

Resources

Latest Media 20

Subtitle
Learn More
Add to myAnalog