How to Easily Neutralize Overvoltages with a Protective Circuit

Jun 17 2024

Abstract

In many applications, it is crucial to safeguard against overvoltages. This article explains how overvoltages can be neutralized with a protective circuit.

Introduction

Overvoltages can be caused, for example, by the rapid switching off of a high load in a power distribution system. Surge protection is recommended to protect other loads that are connected to the same power supply. Figure 1 shows the arrangement of a protection circuit, using the LT4363 in front of the electronic circuit to be protected. The example is from an industrial application where the nominal supply voltage is 24 V.

Figure 1. A simplified illustration of a surge protection circuit used for intercepting a voltage surge.

Figure 1. A simplified illustration of a surge protection circuit used for intercepting a voltage surge.

Normally, the electronics to be protected should continue to operate without interruption during an overvoltage. This requires the protective circuit to operate the circuit breaker (Q1 in Figure 1) in the linear range. The MOSFET is neither switched off nor switched on during the occurring overvoltage. It is partially switched on. In this operating state, it behaves like a resistor across which the overvoltage drops. The energy of the increased voltage is thus converted into heat in MOSFET Q1. Depending on the selection of the MOSFET, it can only withstand this heat for a certain time before it is destroyed by excessive heat.

Figure 2 shows a typical safe operating area (SOA) curve of a MOSFET. This curve defines how long the device can carry which current at which voltage drop. If you want a higher current to flow through the MOSFET for a longer period, a larger MOSFET with a larger SOA range must be selected. The larger the SOA range, the larger the MOSFET. This also increases the cost of the component.

Figure 2. A typical SOA curve of a MOSFET.

Figure 2. A typical SOA curve of a MOSFET.

To size the component optimally, an attempt is made to operate the smallest possible MOSFET safely. This means that it is not oversized and yet a large part of its SOA can be used in the application. This requires the controller IC to precisely recognize the operating state to determine whether the operation is taking place in the safe range of the SOA. However, many controller ICs only measure the current flowing through the MOSFET. It is better to also know the voltage drop across the MOSFET.

An LT4363 surge protector component not only considers the level of the current through the MOSFET, but also the voltage applied between the source and drain. This means that the MOSFET can be operated more safely in linear mode. This can lead to the selection of a smaller MOSFET and lower system costs.

The protection mechanism works by charging the timer capacitor at the TMR pin in Figure 1, depending on the measured current and the measured drop-out voltage. If the voltage at the capacitor rises above 1.275 V, a warning is generated. Above 1.375 V, the MOSFET is switched off completely to protect it.

Figure 3 shows how the voltage on the timer capacitor of the LT4363 in Figure 1 rises due to the VDS voltage on the MOSFET Q1 in Figure 1. There is a similar charging diagram for the current flowing through the MOSFET Q1. These parameters ensure that the SOA curve of a MOSFET is not exceeded. Safe operation and simultaneous overvoltage protection are thus achieved.

Figure 3. A quasi-simulation of an SOA curve in the LT4363 by charging a timer capacitor as a function of the drain source voltage.

Figure 3. A quasi-simulation of an SOA curve in the LT4363 by charging a timer capacitor as a function of the drain source voltage.

Conclusion

Overvoltage protection modules appear quite simple and unspectacular. However, small features can make a big difference in the behavior of the overvoltage protection and in the selection of a suitable MOSFET.

About The Authors

Frederik Dostal
Frederik Dostal is a power management expert with more than 20 years of experience in this industry. After his studies of microelectronics at the University of Erlangen, Germany, he joined National Semiconductor in 2001, w...
Add to myAnalog

Author's Contact Information

Frederik Dostal

Power Management Expert

Related to this Article

Product Categories

Latest Media 20

Subtitle
Learn More
Add to myAnalog