4.5ns Dual-Comparator-Based Crystal Oscillator has 50% Duty Cycle and Complementary Outputs

Figure 1’s circuit uses the LT1720 dual comparator in a 50% duty cycle crystal oscillator. Output frequencies of up to 10MHz are practical.

Figure 1. Crystal oscillator has complementary outputs and 50% duty cycle. A1’s feedback maintains output duty cycle despite supply variations.

Resistors at C1’s positive input set a DC bias point. The 2k–0.068µF path furnishes phase-shifted feedback and C1 acts like a wideband, unity-gain follower at DC. The crystal’s path provides resonant positive feedback and stable oscillation occurs. C2, sensing C1’s input, provides a low skew, complementary output. A1 compares band-limited versions of the outputs and biases C1’s negative input. C1’s only degree of freedom to respond is variation of pulse width; hence, the outputs are forced to 50% duty cycle.

The circuit operates with AT-cut fundamental crystals from 1MHz to 10MHz, over a 2.7V–6V power supply range. 50% duty cycle is maintained at all supply voltages, with output skew below 800 picoseconds. Figure 2 plots skew, which is seen to vary by about 800ps over a 2.7V–6V supply excursion.

Figure 2. Output skew varies only 800ps over a 2.7V–6V supply excursion.

About The Authors

Joseph Petrofsky
Jim Williams
James M. Williams (April 14, 1948 – June 12, 2011) was an analog circuit designer and technical author who worked for the Massachusetts Institute of Technology (1968–1979), Philbrick, National Semiconductor (1979–1982) and...
Add to myAnalog

Author's Contact Information

Joseph Petrofsky

Jim Williams

Related to this Article

Latest Media 20

Subtitle
Learn More
Add to myAnalog