Getting Started with Hall-Effect Sensors Using the MAX9921
Oct 4 2022
Jesvin explains the hall effect and how hall-effect sensors can be useful in applications that require contactless sensors such as an automatic door opener. He then demonstrates the MAX9921, which is the industry’s first two-wire hall-effect sensor.
Getting Started with Hall-Effect Sensors Using the MAX9921
Oct 4 2022
Jesvin explains the hall effect and how hall-effect sensors can be useful in applications that require contactless sensors such as an automatic door opener. He then demonstrates the MAX9921, which is the industry’s first two-wire hall-effect sensor.
{{modalTitle}}
{{modalDescription}}
{{dropdownTitle}}
- {{defaultSelectedText}} {{#each projectNames}}
- {{name}} {{/each}} {{#if newProjectText}}
-
{{newProjectText}}
{{/if}}
{{newProjectTitle}}
{{projectNameErrorText}}