AN038: Using TRINAMIC’s IC Software API and Examples
Introduction
This application note describes the structure of the ADI TRINAMIC software API and how it can be used to simplify and speed up your firmware development based on hardware with ADI TRINAMIC motion control chips. The software API is part of the Technology Access Package (TTAP) [1][2], a comprehensive collection of technical support information and tools for ADI TRINAMIC’s chip and module solutions. This application note explains which compiler and tools can be used to compile the TMC-EvalSystem project and how to upload the firmware to a module using a third-party programmer or the standard bootloader with the TMCL-IDE.
Software API Project Structure
The API is designed for C applications and can be used for different CPU types. For example, the API is used for ADI TRINAMIC’s modular evaluation system boards called Landungbrücke (Freescale MK20 cortex M4 processor) [5] and Startrampe (STM-F205 cortex M3 processor) [6].
The API is structured as shown in figure 1:

Figure 1. TMC-API structure.
The folder tmc/helpers contains general definitions for data types and bit handling, independent of the processor used. The folder tmc/ic contains a folder for each ADI TRINAMIC chip, e.g. tmc/ic/TMC4670. Each of these folders contain a header file with the chip’s register address list (e.g., TMC4670_Register.h). Another .h and .c file (e.g., TMC4670.h/.c) provide low level, mid level, and high level functions for the specific chip. Low level functions are necessary for SPI read and write access. Mid level functions like setTargetVelocity(...) or getActualPosition() demonstrate the typical register access for different application scenarios, e.g., for velocity or position mode. For some chips, there are also functions for encoder initialization and real-world current scaling available.
The next chapter shows the use of the API in a firmware project on the example of the ADI TRINAMIC evaluation board firmware project for Landungbrücke and Startrampe.
Evaluation Board Project Structure
The evaluation board project demonstrates the usage of the TMC-API and can be used as starting point for your own firmware development. It should be an example for you to simplify and speed up firmware development based on hardware with ADI TRINAMIC motion control ICs. The structure of the evaluation board project is shown in figure 2:

Figure 2. TMC Eval System structure.
The evaluation board project is a makefile project and supports two processor types: a Freescale MK20 (cortex M4 processor used in the Landungbruecke) [5] and a STM-F205 (cortex M3 processor) [6]. The processor can be selected according to a build-command for the makefile. The complete firmware project is provided anf is available for free use and adaption [2]. The project uses the Eclipse IDE for C/C++ developers and can be extended for further processor types and evaluation boards.
On top of the CPU specific firmware part, a hardware abstraction layer has been implemented to abstract the access to digital IO, the ADC measurement, SPI, communication, PWM, and eval board detection from the CPU specific firmware part. The eval board firmware detects connected eval boards automatically and loads a board specific firmware part dynamically corresponding to the actual connected eval board. This firmware part uses the TMC-API for the header file and the *.h/*.c file for the specific functionality of the actual used ADI TRINAMIC motion control IC. Using the hardware abstraction layer, each eval board has access to a wide range of CPU functions in a CPU independent way.
Requirements and Installation Guide
This section describes the list of tools needed to compile the firmware project and upload it to the Landungsbrücke or Startrampe. For the installation and configuration, a step-by-step guide with screenshots is presented.
Tools
These are the software packages you need in order to use the TMC-API in your project:
- Eclipse: An open-source integrated development environment (IDE)
- GNU ARM Embedded Toolchain: Pre-built GNU toolchain for ARM Cortex-M processors
- TMCL-IDE: The visual software to control and update TRINAMIC modules and evaluation boards

Eclipse
Eclipse is used to organize, program and compile your software projects. Other IDE’s can be used instead, but the TMC-API project was developed with it and the Eclipse project files are provided along with the code.
Please download the latest version of Eclipse from https://eclipse.org/downloads/, choose the package “Eclipse IDE for C/C++ Developers” as shown on figure 3, and follow the installation wizard.

Figure 3. Eclipse package selection.
For older versions of Eclipse or other installation methods, it is necessary to either download the “Eclipse IDE for C/C++ Developers” package directly or install the Eclipse CDT plugin, available at https://eclipse.org/cdt/.
GNU ARM Embedded Toolchain
The GNU ARM Embedded GCC can be used to compile the firmware. You can download the most recent release here: https://launchpad.net/gcc-arm-embedded/+download. Please follow the installation wizard to set up the toolchain in your system.
TMCL-IDE
The TMCL-IDE software tool is developed by ADI TRINAMIC and offers many tools and wizards to control various ADI TRINAMIC modules and evaluation board products. You can use the TMCL-IDE to update the firmware of a ADI TRINAMIC evaluation board. Please download the latest TMCL-IDE release here: http://www.trinamic.com/support/software/ and install it in your system.
If you want to update the firmware of a module without bootloader feature (e.g., self-designed boards), you will need a programmer device. The following are two common options for some of the most popular embedded processor families:
- ST-LINK: In-circuit debugger and programmer for STM8 and STM32 MCUs
http://www.st.com/en/development-tools/st-link.html - Segger J-Link: USB powered JTAG debug probe supporting a large number of CPU cores
https://www.segger.com/jlink-debug-probes.html
How to create and update a new firmware image
This section explains the steps you need to follow in order to set-up the programming environment to use the ADI TRINAMIC TMC-API project. Afterwards, you can create your own firmware image and update it to an ADI TRINAMIC evaluation board.
- Download TMC-API [3] and TMC-EvalSystem [4] projects
- Download TTAP from the ADI TRINAMIC website [2]
- Configure GNU Toolchain
- Import TMC-API and TMC-EvalSystem Eclipse projects
- Build the firmware
- Update your evaluation board
Download TMC-API and TMC-EvalSystem from the ADI TRINAMIC website
You can download the ADI TRINAMIC TMC-API [3] and TMC-EvalSystem [4] source code projects from the ADI TRINAMIC website for free use and adaption. Extract the *.zip files “TMC-API.zip” and “TMC-EvalSystem.zip” to a folder of your system.
Configure GNU Toolchain
The makefile of the TMC-EvalSystem project uses “cs-make.exe” and “cs-clean.exe”. You can find these files in the folder “Firmware/Toolchain” within the TTAP package [3]. Copy these files and browse to the installation folder of the GNU ARM Toolchain (which you have installed in Section 2.1.2). The path of the folder should be like “C:\Program Files (x86)\GNU Tools ARM Embedded\5.4 2016q2” (where “5.4” is the installed version and “2016q2” the release date). Open sub-folder “bin” and paste the files “cs-make.exe" and “cs-clean.exe" there.
Afterwards, the “bin” folder of the compiler (the folder where the files were copied) must be added to the Windows PATH variable. The process may differ between Windows versions. In Windows 10, search for and select “System (Control Panel)”. Click the advanced system settings link and then click on Environment Variables. Select the PATH environment variable and select it. Then click Edit as shown in Figure 4. If the PATH environment variable does not exist, click New. Otherwise, add the path to the “bin” folder as shown in the figure.

Figure 4. Add folder to PATH variable.
Import TMC-API and TMC-Evalsystem Eclipse projects
Open Eclipse, choose a workspace path and click on “Workbench” to close the welcome screen. Next, click on File - Import and choose “Existing Projects into Workspace” under “General” as shown in figure 5. Then click on “Next”.

Figure 5. Import TMC-API.
Click on “Browse" and choose the path where you have downloaded the TMC-API and TMC-EvalSystem projects. Select “TMC-API” and “TMC-EvalSystem” and check “Copy projects into workspace”. Proceed with “Finish” as shown in figure 6.

Figure 6. Copy TMC-API to workspace.
Now you have imported both projects containing the source code into Eclipse. You can choose a file and start to edit the file. For example, in the left panel, open the TMC-EvalSystem project and double click on main.c to open the file. The source code will be shown on the central panel as shown in figure 7.

Figure 7. Build Firmware Image.
Build firmware
At this point, you are ready to build the firmware image. Click on the project “TMC-EvalSystem” to select it. To start the compilation, you have to find “Build Targets” on the top right panel. In new Eclipse releases, you can also find it on the file tree view under the project name shown in figure 7.
Select the appropriate target for your board. If you have a Landungsbrücken evaluation board, double-click on “Landungsbruecke_BL” (as highlighted in the image). If your board is a Startrampe evaluation board, double-click on “Startrampe_BL”. In the console (bottom panel) you will see the compile output finished with a “Build finished” message when the process finishes successfully.
Targets ending with “_NOBL” are for boards without a bootloader. The created firmware images will have to be flashed with a programmer device instead of using the TMCL-IDE firmware update tool.
Update a module
Open the TMCL-IDE software. Power and connect your module. At the first start, the TMCL-IDE will ask you for permission to install the ADI TRINAMIC USB driver.
After installing the driver, your module will appear on the left panel. Click on Tools -> Firmware Update or on its icon on the top-right toolbar (an arrow pointing down, highlighted in figure 8). Check that the selected module is correct and click on “Browse” to find your firmware image.

Figure 8. TMCL-IDE Browse image file.
Move to your Eclipse workspace path and open the build folder of your module inside the TMC-EvalSystem project. There you will find a .hex file whose name indicates your module and firmware version.
Figure 8 shows an example with a Landungsbrücke evaluation board. You can see that the selected module matches the one shown on the left panel. The “TMC-EvalSystem” path appears in the smaller window. There, the “Landunsbruecke_2.91_BL.hex” file from the “_build_Landungsbruecke” folder is selected.
If the firmware image is compatible with the module, you can click on “Update” as shown in figure 9.

Figure 9. TMCL-IDE Update image file.
For a non-bootloader firmware image, connect your programmer device to your PC and your module (e.g., via USB and JTAG respectively). Configure the programmer software for your module’s processor and open the “_NOBL” .hex. Connect to the processor and proceed to flash the image.
Afterwards, please reboot your module and have fun with the evaluation board or your own designed module.
References
[1] TRINAMIC, “AN37: TRINAMIC Technology Access Package” www.trinamic.com/support/help-center/downloads/AN037-TRINAMIC_Technology_Access_Package
[2] “TRINAMIC Technology Access Package (TTAP)” www.trinamic.com/support/software/
[3] TRINAMIC, “TMC-API eclipse project” www.trinamic.com/support/software/
[4] TRINAMIC, “TMC-EvalSystem eclipse project” www.trinamic.com/support/software/
[5] TRINAMIC, ”Landungsbruecke evaluation board” www.trinamic.com/support/eval-kits/details/landungsbruecke/
[6] TRINAMIC, ”Startrampe evaluation board” www.trinamic.com/support/eval-kits/details/startrampe/