Maximizing Cell Monitoring Accuracy and Data Integrityin Energy Storage Battery Management Systems
Maximizing Cell Monitoring Accuracy and Data Integrityin Energy Storage Battery Management Systems
2015-08-07
Grid-connected battery arrays are viable backup and carry-through power sources; application-specific measurement ICs which meet their unique and sophisticated requirements ensure reliable system performance.
The use of large-scale battery arrays for backup and carry-through energy storage is getting increasing attention, as evidenced by Tesla Motors' recent announcement of their Powerwall system for homes and offices. The batteries in these systems are continually charged from the power-line grid or other source, and then deliver AC-line power back to the user via a DC/AC inverter.
Using batteries for power backup is not new, with many systems spanning basic 120/240Vac and several hundred watts for short-term desktop-PC backup, to thousands of watts for specialty vehicles, such as ships, hybrid cars, or all-electric vehicles, up to hundreds of kilowatts for grid-scale telecom and data-center backup (see Figure 1). Yet while advances in battery chemistry and technology get much of the attention, an equally critical part of a viable battery-based installation is its battery management system (BMS).

Figure 1. Battery-Based Backup Is Well-Suited for Fixed and Mobile Applications Spanning Thousands of Watts to Hundreds of kW, and Can Provide Reliable, Effective Power Across a Wide Range of Applications.
There are many challenges when implementing battery management systems for energy storage, and their solutions do not simply scale up from small-scale, lower-capacity battery packs. Instead, new and more sophisticated strategies and critical support components are needed.
The challenge begins with the need for high accuracy and confidence in the many measurements of key battery cell parameters. Further, the design must be modular in its subsystems to enable tailoring the configuration to the specific needs of the application, along with possible expansion, overall management issues, and necessary maintenance.
The operating environment of larger-scale storage arrays brings other significant challenges, as well. The BMS must provide precise, consistent data within an extremely noisy electrical and often hot environment despite the high voltage/current inverters and resultant current spikes. In addition, it must provide extensive fine-grain data on internal module and system temperature measurements, which are critical for charging, monitoring, and discharging, rather than just a few broad-brush aggregate values.
Due to the basic role of these power systems, their operating reliability is inherently critical. To translate that easily stated objective into reality, the BMS must ensure data accuracy and integrity, along with continuous health assessments so it can take the needed actions on an ongoing basis. Achieving a robust design and safety is a multi-level process, and the BMS must anticipate problems, perform self-test, and provide failure detection on all subsystems, then implement appropriate actions while in standby and operational modes. As a final mandate, due to the high voltage, current, and power levels, there are many stringent regulatory standards that the BMS must meet.
System Design Translates Concepts to Real-World Results
Although monitoring rechargeable batteries is simple in concept – just place the voltage- and current-measurement circuits at the cell terminals – the reality of a BMS is quite different and much more complicated.
Robust design begins with comprehensive monitoring of individual battery cells, which places significant demands on analog functions. The cell readings need millivolt and milliamp accuracy, and voltage and current measurements must be time-synchronized to calculate power. The BMS must also assess validity of each measurement, as it needs to maximize data integrity, while it must also identify errors or questionable readings. It cannot ignore unusual readings which may indicate a potential problem, but at the same time, it should not take action based on data which has errors.
A modular BMS architecture enhances robustness, scalability, and reliability. Modularity also facilitates use of isolation where needed in the data links between subsections to minimize impact of electrical noise and to enhance safety. In addition, advanced data-encoding formats including CRC (cyclic redundancy check) error detection and link-acknowledgement protocols assure data integrity, so the system management function has confidence that the data it receives is what was sent.
An example of a BMS that incorporates these principles is the scalable and customizable battery management system developed by Nuvation Engineering (Waterloo, Ontario and Sunnyvale, CA). The Nuvation BMS design is proving itself with design wins in grid energy-storage systems and power-backup equipment, where reliability and ruggedness are critical. The key advantage of this off-the-shelf BMS is its tiered, hierarchical topology (Figure 2) with three subsystems, each with unique functions, as shown in Figure 3.
- The cell interface provides tight management and monitoring of each battery cell in a stack; the system uses as many cell interfaces as needed, depending on the number of stacks. These interfaces can be daisy-chained as the number of cells and thus the stack voltage increases.
- The cell interface is connected to a single stack controller which monitors and manages multiple cell-interface units. Multiple stack controllers can be connected together, if needed, to support large packs with many stacks in parallel.
- The power interface connects the stack controllers to high voltage/current lines and is the interface to the inverter/charger. It isolates high-voltage and high-current components of the stack physically and electrically from the other modules. It also powers the BMS directly from the battery stack, thus eliminating the need for any external power supplies for the BMS operation.
The modular and hierarchical architecture of the Nuvation BMS supports battery-pack voltages ranging up to 1250Vdc, using cell-interface modules, each containing up to 16 cells, stacks with up to 48 cell-interface modules, and battery packs that contain multiple stacks in parallel. The entire array assembly is managed as a single unit from the user's perspective.

Figure 2. The Nuvation Engineering Battery Management System Is the Interface Between the AC Power Grid and an Array of Battery Cells; it Provides Both Sophisticated Battery Charging/Discharge Oversight as Well as the DC/AC Inverter Function.

Figure 3. The Three Major Subsystems of the Nuvation BMS—Cell Interface, Stack Controller, Power Interface—Comprise a Modular, Hierarchical Design Which Results in Scalability, Robustness, and Reliability Across a Wide Range of Power Levels.
Solid Design Builds from the Bottom Up
Factors such as modular architecture, hierarchical topology, and error-aware design are essential to the integrity and expandability of the Nuvation BMS, but not enough. A successful implementation requires high-performance functional blocks to serve as the physical foundation.
That's why the LTC®6804 Multicell Battery Monitor IC from Linear Technology (Figure 4) plays a critical role in the Nuvation BMS implementation. It is expressly tailored for the needs of BMS systems and multicell designs, beginning with providing precise measurements of up to 12 battery cells stacked in series. Its measurement inputs are not ground-referenced, which greatly simplifies measurement of those cells, and the LTC6804 itself is stackable for use with higher-voltage arrays (and it also supports a variety of cell chemistries). It offers maximum 0.033% error with 16-bit resolution, and needs just 290μs to measure all 12 cells in the stack. Such synchronized voltage and current measurements are critical to yield meaningful analysis of power parameters.

Figure 4. The LTC6804 Multicell Battery Monitor IC from Linear Technology Provides Accurate, Precise Measurements On Stacked Battery Cells, Which Are the Starting Point for a Successful BMS Implementation.
Of course, performance in the benign environment of a prototype at the bench is not the same as actual achievable performance in an electrically and environmentally hostile real-world BMS setting. The LTC6804's analog/digital converter (ADC) architecture is designed to resist and minimize those detrimental effects, using filters specifically designed for the noise of power inverters.
The data interface uses a single twisted-pair, isolated SPI interface which supports rates up to 1Mb and distances of up to 100 meters. To further enhance system integrity, the IC includes an array of ongoing subsystem tests. As further indication of its reliability and ruggedness, the LTC6804 meets the stringent AEC-Q100 standard for automotive quality. This IC achieves its results due to an application-specific design which focuses closely on BMS issues and environments, including the unique system-level objectives of the application and its many challenges.
Three Major Issues Resolved
The LTC6804 addresses three major areas which affect system performance, conversion accuracy, cell balancing, and connectivity/data-integrity considerations:
1. Conversion Accuracy
Due to the short- and long-term accuracy demands of the BMS application, it uses a buried-Zener conversion reference rather than a bandgap reference. This provides a stable, low-drift (20ppm/√kHr), low-temperature coefficient (3ppm/°C), low-hysteresis (20ppm) primary voltage reference along with excellent long-term stability. This accuracy and stability is critical since it is the basis for all subsequent battery-cell measurements and these errors have a cumulative impact on acquired-data credibility, algorithm consistency, and system performance.
Although a high-accuracy reference is a necessary feature to ensure superior performance, that alone is not enough. The A/D converter architecture and its operation must meet specifications in an electrically noisy environment, which is the result of the pulse-width modulated (PWM) transients of the system's high current/voltage inverter. Accurate assessment of the state of charge (SOC) and health of the batteries also requires correlated voltage, current, and temperature measurements.
To mitigate the system noise before it can affect the BMS performance, the LTC6804 converter uses a delta-sigma topology, aided by six user-selectable filter options to address noisy environments. The delta-sigma approach reduces the effect of electromagnetic interference (EMI) and other transient noise, by its very nature of using many samples per conversion, with an averaging, filtering function.
2. Cell Balancing
The need for cell balancing is an unavoidable consequence in any system that uses large battery packs arranged as groups of cells or modules. Although most lithium cells are well matched when first acquired, they lose capacity as they age. The aging process can differ from cell to cell due to a number of factors, such as gradients in pack temperature. Exacerbating the whole process, a cell that is allowed to operate beyond its SOC limits will prematurely age and lose additional capacity. These differences in capacity, combined with small differences in self-discharge and load currents, lead to cell imbalance.
To remedy the cell imbalance issue, the LTC6804 directly supports passive balancing (with a user-settable timer). Passive balancing is a low cost, simple method to normalize the SOC for all cells during the battery charge cycle. By removing charge from the lower capacity cells, passive balancing ensures these lower capacity cells are not over-charged. The LTC6804 can also be used to control active balancing, a more complicated balancing technique which transfers charge between cells through the charge or discharge cycle.
Whether done using active or passive approaches, cell balancing relies on high measurement accuracy. As measurement error increases, the operating guardband which the system establishes must also be increased, and therefore the effectiveness of the balancing performance will be limited. Further, as the SOC range is further restricted, the sensitivity to these errors also increases. The LTC6804's total measurement error of less than 1.2mV is well within system-level requirements.
3. Connectivity/Data Integrity Considerations
Modularity in the battery-pack design adds to scalability, serviceability, and form-factor flexibility. However, this modularity requires that the data bus between packs has galvanic isolation (no ohmic path), so failures in any one pack do not affect the rest of the system or put high voltages on the bus. Further, the wiring between packs must tolerate high levels of EMI.
A two-wire isolated data bus is a viable solution to achieve these goals in a compact and cost-effective way. Therefore, the LTC6804 offers an isolated SPI interconnect called iso-SPI, which encodes the signals for clock, data in, data out, and chip select into differential pulses, which are then coupled through a transformer, a rugged, reliable, and long-established isolation component (Figure 5).

Figure 5. The LTC6804 Supports an Isolated SPI Interface Which Can Be Daisy-Chained for Larger Arrays, Resulting in a Robust, EMI-Resistant Interconnect That Minimizes Cabling Requirements and the Number of Isolators.
Devices on the bus can be connected in a daisy chain configuration, which greatly reduces harness size and enables modular designs for large, high-voltage battery packs, while maintaining high data rates and low EMI susceptibility (Figure 6).

Figure 6. Test Results on the LTC6804 and isoSPI Interface Showed No Data Errors Despite 200mA of Injected RF with the isoSPI Operating at 20mA Signal Strength.
To demonstrate the noise immunity, Linear Technology performed BCI testing on the LTC6804. This involved coupling 100mA of RF energy into the battery-wiring harness, with the RF carrier swept from 1MHz to 400MHz and with 1kHz AM modulation on the carrier. The LTC6804 digital filter was programmed for a 1.7kHz cutoff frequency, and an external RC filter and ferrite choke were added as well. The result: the error in voltage reading was below 2mV over the entire RF sweep range.
An array of self-assessment and self-test features adds to the suitability of the LTC6804 for BMS applications. These checks include open-wire detection; a second internal reference for ADC clock; multiplexer self-test, and even measurement of its internal power-supply voltages. The device is engineered for systems that are intended to be compliant with ISO 26262 and IEC 61508 standards.
Conclusion
There’s a lot of glamour associated with back-up and carry-through supplies for grid-level systems. It seems so straightforward: just keep an array of batteries charged (whether from the grid-AC line, or solar, wind, or other renewable sources), then use the batteries with a DC/AC inverter when you need to provide line-equivalent AC power.
The reality is that batteries are not simple in any of their behavior or performance characteristics, and they need carefully controlled charging, monitoring of their voltage, current, and temperature, and discharging. As power levels increase, a practical, efficient, and safe system is not a trivial design, and so a grid-connected multicell BMS is a complex system. Many unique problems need to be understood and addressed, with safety a major concern as well.
A successful and viable system design needs a modular, structured, top-down architecture that is supported from bottom up by optimized components such as the LTC6804. When combined with sophisticated, secure data-acquisition and control software, the result is a high-performance, reliable BMS that requires minimal operator involvement, and will function autonomously for years of reliable service.
关于作者
关联至此文章
{{modalTitle}}
{{modalDescription}}
{{dropdownTitle}}
- {{defaultSelectedText}} {{#each projectNames}}
- {{name}} {{/each}} {{#if newProjectText}}
-
{{newProjectText}}
{{/if}}
{{newProjectTitle}}
{{projectNameErrorText}}