利用DS1841对数电阻优化雪崩光电二极管(APD)的偏置范围

2008-09-05

Figure 1

   

摘要

本文阐述了如何使用DS1841对数电位器调节APD偏置电路的输出范围。为了使调节过程更简单,本文还提供了电子数据表。

APD偏置电路

DS1841可受温度控制的非易失(NV)、I²C对数电位器包含了一个7位对数变化的电阻器。通过与升压型DC-DC转换器相配合,DS1841能够调节施加在雪崩光电二极管的偏置电压。利用三个外部电阻(RSER、RTOP和RPAR)调节输出范围(图1)。

图1. 利用DS1841和升压型DC-DC转换器(此处为MAX5026或MAX1523)构成的APD偏置电路
图1. 利用DS1841和升压型DC-DC转换器(此处为MAX5026或MAX1523)构成的APD偏置电路

调节APD偏置电压范围

利用电子数据表DS1841 APD偏置电压调节(xls)可以方便地调节APD偏置电压。该电子数据表包含四个输入变量:RTOP、RSER、RPAR以及VFB。输入这些电阻值后,电子数据表即可计算出四个输出值:VAPD (最大值)、VAPD (最小值)、STEP (最大值)和STEP (平均值)。此外还生成了两个曲线图:APD偏置与DAC码关系曲线和每级电压与DAC码的关系曲线图。图2所示界面给出了四个变量以及通过输入值而生成的图形。表1定义了电子数据表所使用的参数。

图2. 该电子数据表界面包含了四个数据输入变量(见左上角)
图2. 该电子数据表界面包含了四个数据输入变量(见左上角)

表1. 使用DS1841调节APD偏置电压范围时的变量定义

VFB The voltage present at the feedback node of the DC-DC converter.
VAPD (max) The maximum voltage to which the APD bias can be set under worst-case conditions.
VAPD (min) The minimum voltage to which the APD bias can be set under worst-case conditions.
STEP (max) The maximum calculated voltage step that can occur between two adjacent DAC codes.
STEP (avg) The average voltage step size that occurs across the full range.
VSTEP +20% The voltage step size when the variable resistor is at the maximum of the process range (+20%).
VSTEP -20% The voltage step size when the variable resistor is at the minimum of the process range (-20%).
VAPD +20% The APD bias voltage when the variable resistor is at the maximum of the process range (+20%).
VAPD -20% The APD bias voltage when the variable resistor is at the minimum of the process range (-20%).

关联至此文章

产品

产品分类

最新视频 21

Subtitle
了解更多
3