摘要
当需要增加网络保护元件,或需要通过连接器和其它PCB路由信号时,常常需要调整发送信号波形。DS26528和DS26524能够对输出脉冲进行细小的或重要的调整。本应用笔记介绍了访问工厂测试寄存器、调整发送信号波形的方法,以满足多种应用需求。
T1和E1发送波形的可编程段
通过DS26528和DS26524的内部寄存器,可以对发送脉冲的两个主要属性进行控制:幅度和定时。T1和E1发送脉冲分为几段,每段都可以单独控制,以提供所要求的信号波形。图1显示了T1脉冲的分段,以及控制每一段的寄存器。图2为E1脉冲的类似信息。
T1和E1发送波形的幅度控制
控制DS26528和DS26524发送脉冲幅度的方式有以下两种:
- 调整DAC增益
利用L1TXLAE寄存器的DAC[3:0]位可同时对T1或E1电平进行正向和负向调整。 - 局部波形电平调整
通过Level Adjustment寄存器中的WLA[3:0]位,可对波形的特定段进行微调。电平调整的步长与设置的DAC增益成比例。如果DAC增益提高10%,则步长也相应增加10%。
T1和E1发送波形计定时控制
DS26528和DS26524发送脉冲的定时由Level Adjustment寄存器的CEA[2:0]位控制,可以正向或负向调整各个边沿,增量为TCLK的1/32。
一般性建议
调整DAC增益是控制发送脉冲幅度的最简单方法,因为只修改一个寄存器便可以控制整个波形。在进行波形调整时首先调整DAC增益,然后再调整各个独立的Level Adjustment寄存器(如果需要的话),以获得满足要求的波形,这样可以使总的调整步骤最少。
DAC的最大输出将受VDD的影响,VDD较低时,也许很难达到最大DAC增益设置。改变VDD也会影响线驱动器输出级的最大电压。
负值不用带符号的整数表示,MSB是标志位,LSB代表幅度,与符号无关。例如,-3在WLA[3:0]寄存器中表示为1011b (第3位为1代表负数,接下来三位011是数值大小:3),而不是1101b (4位带符号整数)。
图1. T1脉冲分段控制
T1脉冲分段控制
- 过冲(1) -- 寄存器L1TXLAA WLA[4:0]
- 时钟沿(1CE) -- 寄存器L1TXLAA CEA[2:0]
- (1CE) = 从过冲至平台的时钟沿跳变
- 平台(2) -- 寄存器L1TXLAB WLA[4:0]
- 时钟沿(2CE) -- 寄存器L1TXLAB CEA[2:0]
- (2CE) = 从平台至下降沿时钟沿跳变
- 下冲(3) -- 寄存器L1TXLAC WLA[4:0]
- 时钟沿(3CE) -- 寄存器L1TXLAC CEA[2:0]]
- (3CE) = 下降沿至下冲(3)结束的时钟沿
- 下冲(4) -- 寄存器L1TXLAD WLA[4:0]
- 时钟沿(4CE) -- 寄存器L1TXLAD CEA[2:0]
- (4CE) = 下冲结束(3)至下冲恢复(4)的时钟沿
- 下冲(5) -- 寄存器L1TXLAC WLA[4:0]
- (1CE) = 从过冲至平台的时钟沿跳变

图2. E1脉冲分段控制
E1脉冲分段控制
- 过冲(1) -- 寄存器L1TXLAA WLA[4:0]
- 时钟沿(1CE) -- 寄存器L1TXLAA CEA[2:0]
- (1CE) = 过冲至平台的时钟沿
- 平台(2) -- 寄存器L1TXLAB WLA[4:0]
- 时钟沿(2CE) -- 寄存器L1TXLAB CEA[2:0]
- (2CE) = 平台至下降沿的时钟沿跳变
- (1CE) = 过冲至平台的时钟沿
注意:
EI模式中未用到寄存器L1TXAC、L1TXAD和L1TXAE。
DS26528和DS26524的LIU测试寄存器
表1提供了LIU 1的寄存器地址和说明,这些寄存器被复制为LIU 2至8; 表2提供所有LIU测试寄存器的地址。DS26524不包含LIU 5至8。
表1. LIU 1测试寄存器
Address | Abbr | Description |
1008h | L1TXLAA | LIU 1 Tx Level Adjust A (Test Register) |
1009h | L1TXLAB | LIU 1 Tx Level Adjust B (Test Register) |
100Ah | L1TXLAC | LIU 1 Tx Level Adjust C (Test Register) |
100Bh | L1TXLAD | LIU 1 Tx Level Adjust D (Test Register) |
100Ch | L1TXLAE | LIU 1 Tx Level Adjust E (Test Register) |
表2. LIU测试寄存器地址范围
LIU | Address Range |
1 | 1008 - 100Ch |
2 | 1028 - 102Ch |
3 | 1048 - 104Ch |
4 | 1068 - 106Ch |
DS26528 Only | |
5 | 1080 - 108Ch |
6 | 10A8 - 10ACh |
7 | 10C8 - 10DCh |
8 | 10E8 - 10ECh |
LIU测试寄存器文件说明
下文给出了LIU 1的寄存器地址和说明。这些寄存器被复制为LIU 2至8。所有LIU测试寄存器的地址参见表2。
Register Name: | L1TXLAA |
Register Description: | LIU Tx Level Adjust A (Overshoot Voltage) |
Register Address: | 1008H |
Read/Write Function: | R/W |
Bit # | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
Name | WLA4 | WLA3 | WLA2 | WLA1 | WLA0 | CEA2 | CEA1 | CEA0 |
Default | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 |
第7位至第3位:发送波形输出电平1调整(WLA[4:0]),幅度从默认值±360mV开始调整。
第7位 = 符号位('1'表示负)第2位至第0位:时钟沿调整(CEA[2:0]),时钟沿从默认值移动±3 32x-clk
第6位至第3位 = 数值(无符号)
例如:LSB步长为24mV。
<2> = 符号位('1'表示负)
<1:0> = 时钟沿移动32x-clk (无符号)
Register Name: | L1TXLAB |
Register Description: | LIU Tx Level Adjust B (Plateau Voltage) |
Register Address: | 1009H |
Read/Write Function: | R/W |
Bit # | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
Name | WLA4 | WLA3 | WLA2 | WLA1 | WLA0 | CEA2 | CEA1 | CEA0 |
Default | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 |
第7位至第3位:发送波形输出电平2调整(WLA[4:0]),幅度从默认值±360mV开始调整。
第7位 = 符号位('1'表示负)第2位至第0位:时钟沿调整(CEA[2:0]),时钟沿从默认值移动±3 32x-clk。
第6位至第3位 = 数值(无符号)
例如:LSB步长为24mV
<2> = 符号位('1'表示负)
<1:0> = 时钟沿移动32x-clk (无符号)
Register Name: | L1TXLAC |
Register Description: | LIU Tx Level Adjust C (Undershoot Voltage #1) |
Register Address: | 100AH |
Read/Write Function: | R/W |
Bit # | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
Name | WLA4 | WLA3 | WLA2 | WLA1 | WLA0 | CEA2 | CEA1 | CEA0 |
Default | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 |
第7位至第3位:发送波形输出电平3调整(WLA[4:0])。在±360mV范围内调整默认幅度。
第7位 = 符号位('1'表示负)第2至0:时钟沿调整(CEA[2:0])。时钟沿从默认值移动±32x-clk。
第6位至第3位 = 数值(无符号)
例如:LSB步长为24mV
<2> = 符号位('1'表示负)
<1:0> = 时钟沿移动32x-clk (无符号)
Register Name: | L1TXLAD |
Register Description: | LIU Tx Level Adjust D (Undershoot Voltage #2) |
Register Address: | 100BH |
Read/Write Function: | R/W |
Bit # | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
Name | WLA4 | WLA3 | WLA2 | WLA1 | WLA0 | CEA2 | CEA1 | CEA0 |
Default | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 |
第7位至3:发送波形输出电平4调整(WLA[4:0]),幅度从默认值±360mV开始调整。
第7位 = 符号位('1'表示负)第2至0:时钟沿调整(CEA[2:0])。时钟沿从默认值移动±3 32x-clk。
第6位至第3位 = 数值(无符号)
例如: LSB步长为24mV
<2> = 符号位('1'表示负)
<1:0> = 时钟沿移动32x-clk (无符号)
Register Name: | L1TXLAE |
Register Description: | LIU Tx Level Adjust E (Undershoot Voltage #3) |
Register Address: | 100CH |
Read/Write Function: | R/W |
Bit # | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
Name | WLA4 | WLA3 | WLA2 | WLA1 | WLA0 | CEA2 | CEA1 | CEA0 |
Default | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 |
第7位至4:发送波形输出电平5调整(WLA[3:0]),幅度从默认值±180mV开始调整。
第7位 = 符号位('1'表示负)第3位至第0位:DAC增益调整(DAC[3:0]),修改DAC增益的设置如下。
第6位至第4位 = 数值(无符号)
例如:LSB步长为24mV
0000 - nominal DAC gain (default) |
0001 - DAC gain +2.6% |
0010 - DAC gain +5.3% |
0011 - DAC gain +8% |
0100 - DAC gain +11.1% |
0101 - DAC gain +14.2% |
0110 - DAC gain +17.7% |
0111 - DAC gain +21.3% |
1000 - DAC gain -2.2% |
1001 - DAC gain -4.88% |
1010 - DAC gain -7.11% |
1011 - DAC gain -8.88% |
1100 - DAC gain -11.11% |
1101 - DAC gain -12% |
1110 - DAC gain -15.1% |
1111 - DAC gain -16.4% |
T1和E1发送波形数据
以下数据由DS26528DK得出,能够代表DS26528和DS26524的预期结果。提供这些数据是为了作为一个参考,帮助设计者了解如何利用Level Adjustment寄存器控制T1和E1发送脉冲的幅度和定时,以及能够控制的范围。这些数据在室温以及3.3V VDD条件下获得。
DS26528和DS26524的详细信息
关于Maxim产品的更多信息,请在china.maximintegrated.com/telecom网站查阅器件数据资料。有关Maxim器件进一步的问题,请联系我们的电信应用支持。