Low-noise, Wideband Voltage-controlled Amplifier with "Linear-in-dB" Gain

Low-power, low-distortion, constant-bandwidth AD600 and AD602 duals solve classic VCA problems using new principle

The AD600 and AD602* are dual-channel low-noise, low-distortion voltage-controlled amplifiers (VCAs). Both devices provide a nominal 40-dB gain range, with a 1-dB overrange at each end; for the AD600 the full range is -1 dB to +41 dB; for the AD602, it is -11 dB to +31 dB. Read full article


作者

Barrie Gilbert

Barrie Gilbert

Barrie Gilbert是首位ADI院士,他“付出了毕生精力追求模拟技术的真谛。”他于1972年加入ADI公司,于1979年获封ADI院士,负责管理位于俄勒冈州比佛顿的西北实验室。Barrie于1937年出生于英国伯恩茅斯。在加入ADI公司之前,1954年,他在SRDE工作,研发第一代晶体管,之后加盟Mullard, Ltd.;后来还曾在Tektronix和Plessey研究实验室工作。Barrie是一名IEEE院士(1984年),一生获奖无数。他拥有约50项专利,发表过约40篇论文,与人合作出版多本著作,还是几家期刊的评审人。1997年,他获得了美国俄勒冈州立大学颁发的工程荣誉博士学位。

Generic_Author_image

Bob Clarke

1